This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问zigbee用三个设备测试,一个协调器,一个路由,一个终端,在广播发送一包的时候终端总是收到2包或者3包一样的数据

请问zigbee用三个设备测试,一个协调器,一个路由,一个终端,在广播发送一包的时候终端总是收到2包或者3包一样的数据 ,以前是一些设置,我还需要注意什么么

/****************************************
* The following are for End Devices only
***************************************/

-DRFD_RCVC_ALWAYS_ON=TRUE

/* The number of milliseconds to wait between data request polls to the coordinator. */
-DPOLL_RATE=0

/* This is used after receiving a data indication to poll immediately
* for queued messages...in milliseconds.
*/
-DQUEUED_POLL_RATE=0

/* This is used after receiving a data confirmation to poll immediately
* for response messages...in milliseconds
*/
-DRESPONSE_POLL_RATE=0

/* This is used as an alternate response poll rate only for rejoin request.
* This rate is determined by the response time of the parent that the device
* is trying to join.
*/
-DREJOIN_POLL_RATE=440

XNWK_AUTO_POLL
xPOWER_SAVING