This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power consumption of cc2630

Other Parts Discussed in Thread: CC2630

hello,guys,i have some questions,I want to know that cc2630 uses zstack_ home_ 1.02, making a very simple application that sends 100 bytes of data every 10 minutes in low power mode,in the case of 550mah battery power supply,  how long can it last,maybe Several months or years?

  • 你好,功耗跟个人应用相关,无法具体估算。你可以实测一下你的电流消耗,然后根据电池电压估算时间。实验室测的数据如下:

    – 有源模式 RX:5.9mA
    – 有源模式 TX (0dBm):6.1mA
    – 有源模式 TX (+5dBm):9.1mA
    – 有源模式 MCU:61µA/MHz
    – 有源模式 MCU:48.5 CoreMark/mA
    – 有源模式传感器控制器:
    0.4mA + 8.2μA/MHz
    – 待机电流:1.1μA(RTC 运行,RAM/CPU 保
    持)
    – 关断电流:100nA(发生外部事件时唤醒)
x 出现错误。请重试或与管理员联系。