This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
协议栈zigbee1.2.2a,网关为协调器,即CONCENTRATOR,使用官方ZNP,路由节点使用ZCL协议格式,按swra427c配置设置,ZNP使用CC2530,RAM太少,将MAX_RTG_SRC_ENTRIES减少到90,下面各种路由节点有90个,CONCENTRATOR单播数据可以顺畅的控制路由节点。在ZNP工程的zcl的函数中,zcl_SendCommand()的最后数据发送是AF_DataRequest(),不是AF_DataRequestSrcRtg()!为何在抓CONCENTRATOR发出去的控制包中 source Route Included 项为YES?而不是NO?它是在哪里把源路由表加载进去的?谢谢!