This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

如何在zstack例子simpleApp中添加UART?(CC2530)

在例子simpleApp中

SimpleCollector.c



void zb_ReceiveDataIndication( uint16 source, uint16 command, uint16 len, uint8 *pData )
{
uint8 buf[32];
uint8 *pBuf;
uint8 tmpLen;
uint8 sensorReading;
if (command == SENSOR_REPORT_CMD_ID)
{
…………………………
#if defined( MT_TASK )
debug_str( (uint8 *)buf );
#endif
// can also write directly to uart //如果需要上传至计算机,可自行添加串口发送程序

}
}


【问题一】请问如何添加?

我看一个些文档说,debug_str( (uint8 *)buf );就是串口通信,但是我已经把MT_TASK预编译了,为什么不能在串口调试工具中显示?

【问题二】我曾经在一个TI的点对点测试中成功传输数据,代码如下:

/****************************************************************
初始化串口0函数
****************************************************************/
void initUART0(void)
{
PERCFG = 0x00;
P0SEL = 0x3c; //P0.2和P0.3用作串口
P2DIR &= ~0XC0;
U0CSR |= 0x80;

U0GCR |=0x0A;
U0BAUD |= 216; //波特率设为57600

UTX0IF = 1; //UART0 TX中断标志初始置位1
U0CSR |= 0X40; //串口中断接收允许
IEN0 |= 0x84; //开总中断,接收中断
}
/****************************************************************
串口发送字符串函数
****************************************************************/
void UartTX_Send_String(uchar *Data,int len)
{
int j;
for(j=0;j<len;j++)
{
U0DBUF = *Data++;
while(UTX0IF == 0);
UTX0IF = 0;
}
}

但是在zstack中就没有用了,可能是我移植 的方法不会吧,请问这与zstack中UART有什么区别吗?

十分感谢!