This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1352P 不使用rom里面的bootloader,使用uart1实现一个bootloader,boot和app中ccfg flash和nv flasg如何配置?

collector_2_4g作为app,通过uart1升级cc1352,参考了bim和sensor_oad_onchip_2_4g_secure这两个项目的icf文件配置,分别烧录boot和app代码,运行不起来,使用iar调试模式时,总是弹出如何下图的错误。将boot和app合并起来后,通过flash programmer 2烧录,也运行不起来。icf文件中的ccfg和nv该如何正确配置,附件的是boot和app现在的icf配置文件,请问还需要配置什么?有人做过吗

icf.zip