This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC2592是TI 2.4 GHz射频收发器和范围扩展器。CC2592通过功率放大器(PA)和低噪声放大器(LNA)提供更大的输出功率和更好的接收器灵敏度的,增加了RF链路预算。CC2530与 CC2531有相同的RF前端, 因此此设计对CC2531同样适用。
1.主设计电路:
完整参考电路下载:https://www.ti.com/tool/CC2530-CC2592EM-RD
2.CC2592上有三个数字控制引脚(PA_EN,LNA_EN和HGM)来控制芯片的状态。下表列出了将CC2592连接到CC2530时的控制逻辑:
3.参考设计使用CC2530上的三个GPIO引脚来控制CC2592,LNA_EN必须由RF observation signals控制,而HGM引脚可以由任何GPIO控制,或者与VDD或GND相连。 所使用的I / O引脚如下图所示:
4.软件设置:
1).在编译选项中选择HAL_PA_LNA_CC2592
2). 在程序通过调用API ZMacSetTransmitPower()将输出功率设置为所需的发射功率值.
以下示例显示了在Z-Stack中的Sample Switch Sample Application,使用CC2592 PA-LNA将发射功率设置为15dBm: