This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630 Sensor Controller 功耗

Other Parts Discussed in Thread: CC2630, LAUNCHXL-CC2650

请问下  CC2630 Sensor Controller 功耗问题  ,按手册上说 Active-Mode Sensor Controller: 8.2 µA/MHz, MCU是48-MHz频率  电流应该很小啊,

 我利用Sensor Controller 使用pulse counter和uart emulator时 测了一下,功耗都挺大:

uart emulator打开和关闭相差1.3mA;

pulse counter打开和关闭相差1.1mA

这个功耗算正常吗?