This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2530协调器接入节点设备数量

Other Parts Discussed in Thread: CC2530, CC2630, CC2652R

协议栈home1.2.2a

硬件为cc2530

经过测试默认最大接入终端为20个左右,终端直连协调器

修改NWK_MAX_DEVICE_LIST为50,编译出错,应该是内存不够,但是f8w2530.xcl内存划分,不怎么看懂,请教如何增加XDATA_Z内存空间

Error[e16]: Segment XDATA_Z (size: 0x1fc8 align: 0) is too long for segment definition. At least 0x3c9 more bytes needed. The problem occurred while processing the segment placement command
"-Z(XDATA)XDATA_Z,XDATA_I=_XDATA_START-_XDATA_END", where at the moment of placement the available memory ranges were "XDATA:301-1eff"
Reserved ranges relevant to this placement:
XDATA:1-300 XSTACK
XDATA:301-1eff XDATA_Z
BIT:0-7 BREG
BIT:80-87 SFR_AN
BIT:90-97 SFR_AN
BIT:a0-af SFR_AN
BIT:b8-c7 SFR_AN
BIT:e8-ef SFR_AN
BIT:f8-ff SFR_AN