This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教 Inter-PAN Transaction ID 、PAN ID、 Extended PAN ID的含义及应用

请教  Inter-PAN Transaction ID 、PAN ID、 Extended PAN ID 这三个的定义及分别的应用情景

  • The Extended PAN ID is a network parameter that is new for ZigBee 2007 (EmberZNet 3.x and later) and is used in the ZigBee and ZigBee PRO feature sets. This extended PAN ID [EPID] can be thought of as an extension of the basic, 16-bit PAN ID [PID]. The EPID is a 64-bit value set for the entire network by the ZigBee Coordinator [ZC] at the time the personal area network [PAN] is formed and must not change while the PAN is operating (unlike the PID). Like the PID, all nodes within the same PAN share an EPID.