This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

zclGeneral_SendOnOff_CmdOnDuration这个函数无法使用

zclGeneral_SendOnOff_CmdOnDuration这个函数无法使用,因为  error #20: identifier "COMMAND_ON_DURATION" is undefined

而且在  On/Off Cluster Commands  的定义中也是没有 COMMAND_ON_DURATION这个的定义

  • 你是在哪里使用的?看一下下面的定义,没有找到COMMAND_ON_DURATION的定义的位置

    /*!
     *  Send an On Off Command - COMMAND_ONOFF_ONDURATION
     *  Use like:
     *      ZStatus_t zclGeneral_SendOnOff_CmdOnDuration( uint16_t srcEP, afAddrType_t *dstAddr, uint16_t onDuration, uint8_t disableDefaultRsp, uint8_t seqNum );
     */
    #define zclGeneral_SendOnOff_CmdOnDuration(a,b,c,d,e) zcl_SendCommand( (a), (b), ZCL_CLUSTER_ID_GENERAL_ON_OFF, COMMAND_ON_DURATION, TRUE, ZCL_FRAME_CLIENT_SERVER_DIR, (d), 0, (e), 2, (c) )

  • 我想COMMAND_ON_DURATION應該是對應到ZCL spec的On with timed off (0x42),你可以自己在zcl_general.h加上"#define COMMAND_ON_DURATION 0x42"試試
  • 
    

    我在zclSampleSw_CmdCallbacks里面使用,你说的COMMAND_ON_DURATION自己添加是什么意思?

    添加在下面这里吗??

    /*******************************/
    /*** On/Off Cluster Commands ***/
    /*******************************/
    /// On receipt of this command, a device SHALL enter its 'Off' state.
    #define COMMAND_ON_OFF_OFF                                       0x00
    /// On receipt of this command, a device SHALL enter its 'On' state.
    #define COMMAND_ON_OFF_ON                                        0x01
    /// On receipt of this command, if a device is in its 'Off' state it SHALL
    ///enter its 'On' state. Otherwise, if it is in its 'On' state it SHALL
    /// enter its 'Off' state.
    #define COMMAND_ON_OFF_TOGGLE                                    0x02
    /// The Effect Identifier field is 8-bits in length and specifies the fading
    /// effect to use when switching the device off.
    #define COMMAND_ON_OFF_OFF_WITH_EFFECT                           0x40
    /// The On With Recall Global Scene command allows the recall of the settings
    /// when the device was turned off.
    #define COMMAND_ON_OFF_ON_WITH_RECALL_GLOBAL_SCENE               0x41
    /// The On With Timed Off command allows devices to be turned on for a specific
    /// duration with a guarded off duration so that SHOULD the device be
    /// subsequently switched off, further On With Timed Off commands.
    #define COMMAND_ON_OFF_ON_WITH_TIMED_OFF                         0x42
  • zcl_general.h里面已经定义了COMMAND_ON_DURATION 0x42

    /*******************************/
    /*** On/Off Cluster Commands ***/
    /*******************************/
    /// On receipt of this command, a device SHALL enter its 'Off' state.
    #define COMMAND_ON_OFF_OFF 0x00
    /// On receipt of this command, a device SHALL enter its 'On' state.
    #define COMMAND_ON_OFF_ON 0x01
    /// On receipt of this command, if a device is in its 'Off' state it SHALL
    ///enter its 'On' state. Otherwise, if it is in its 'On' state it SHALL
    /// enter its 'Off' state.
    #define COMMAND_ON_OFF_TOGGLE 0x02
    /// The Effect Identifier field is 8-bits in length and specifies the fading
    /// effect to use when switching the device off.
    #define COMMAND_ON_OFF_OFF_WITH_EFFECT 0x40
    /// The On With Recall Global Scene command allows the recall of the settings
    /// when the device was turned off.
    #define COMMAND_ON_OFF_ON_WITH_RECALL_GLOBAL_SCENE 0x41
    /// The On With Timed Off command allows devices to be turned on for a specific
    /// duration with a guarded off duration so that SHOULD the device be
    /// subsequently switched off, further On With Timed Off commands.
    #define COMMAND_ON_OFF_ON_WITH_TIMED_OFF 0x42

  • COMMAND_ON_DURATION應該是個過渡時期的ZCL command,應該就是對應到COMMAND_ON_OFF_ON_WITH_TIMED_OFF,所以才請你也加上"#define COMMAND_ON_DURATION 0x42"試試
  • YiKai是对的,看名称COMMAND_ON_DURATION似乎是ON的持续时间,你可以用COMMAND_ON_OFF_ON_WITH_TIMED_OFF代替它试试,
    我将与team联系,以确定这个command的含义
  • 嗯,多谢,有回复了,通知我下
  • 可以看一下Ryan在 的回覆

  • 多谢,那看来这个暂时这个commond先不用了
  • 你可以用COMMAND_ON_OFF_ON_WITH_TIMED_OFF代替它
  • 在simpleLink SDK 里面,有没有终端使用ATTRID_ON_OFF_OFF_WAIT_TIME 的例子
  • simpleLink SDK 里面的例程式沒有使用ATTRID_ON_OFF_OFF_WAIT_TIME 的,你要自己嘗試
  • 我这边终端的设置

    1.zclSampleSw_Attrs,其中

    zclSampleSw_OnOff = 0;  

    const uint16_t zclSampleSw_onoff_clusterRevision = 0x0001;

    const uint8_t zclSampleSw_onofftime[5] = {0x00, 0x00,0x01,0x00,0x01};

      // *** On / Off Cluster *** //
      {
        ZCL_CLUSTER_ID_GENERAL_ON_OFF,
        { // Attribute record
          ATTRID_ON_OFF_ON_OFF,
          ZCL_DATATYPE_BOOLEAN,
          ACCESS_CONTROL_READ | ACCESS_REPORTABLE,
          (void*)&zclSampleSw_OnOff
        }
      },
      {
        ZCL_CLUSTER_ID_GENERAL_ON_OFF,
        {  // Attribute record
          ATTRID_CLUSTER_REVISION,
          ZCL_DATATYPE_UINT16,
          ACCESS_CONTROL_READ | ACCESS_CLIENT,
          (void *)&zclSampleSw_onoff_clusterRevision
        }
      },
    
      {
        ZCL_CLUSTER_ID_GENERAL_ON_OFF,
        {  // Attribute record
          ATTRID_ON_OFF_OFF_WAIT_TIME,
          ZCL_DATATYPE_UINT40,
          ACCESS_CONTROL_READ | ACCESS_CLIENT,
          (void *)&zclSampleSw_onofftime
        }
      }

    2.zclSampleSw_CmdCallbacks  里面:

    static void zclonDurationCB(zclOnWithTimedOff_t *pCmd  ){
        printf("zclonDurationCB\n");
    }
    
    
    static zclGeneral_AppCallbacks_t zclSampleSw_CmdCallbacks =
    {
      zclSampleSw_BasicResetCB,               // Basic Cluster Reset command
      NULL,                                   // Identfiy cmd
      NULL,                                   // Identify Query command
      NULL,                                   // Identify Query Response command
      NULL,                                   // Identify Trigger Effect command
    #ifdef ZCL_ON_OFF
      zclonoffCB,                             // On/Off cluster commands
      NULL,                                   // On/Off cluster enhanced command Off with Effect
      NULL,                                   // On/Off cluster enhanced command On with Recall Global Scene
      zclonDurationCB,                        // On/Off cluster enhanced command On with Timed Off
    #endif
    #ifdef ZCL_LEVEL_CTRL
      NULL,                                   // Level Control Move to Level command
      NULL,                                   // Level Control Move command
      NULL,                                   // Level Control Step command
      NULL,                                   // Level Control Stop command
      NULL,                                   // Level Control Move to Closest Frequency command
    #endif
    #ifdef ZCL_GROUPS
      NULL,                                   // Group Response commands
    #endif
    #ifdef ZCL_SCENES
      NULL,                                   // Scene Store Request command
      NULL,                                   // Scene Recall Request command
      NULL,                                   // Scene Response command
    #endif
    #ifdef ZCL_ALARMS
      NULL,                                   // Alarm (Response) commands
    #endif
    #ifdef SE_UK_EXT
      NULL,                                   // Get Event Log command
      NULL,                                   // Publish Event Log command
    #endif
      NULL,                                   // RSSI Location command
      NULL                                    // RSSI Location Response command
    };

    协调器的设置:

    #define zclGeneral_SendOnOff_CmdOnDuration(a,b,c,d,e) zcl_SendCommand( (a), (b), ZCL_CLUSTER_ID_GENERAL_ON_OFF, COMMAND_ON_OFF_ON_WITH_TIMED_OFF, TRUE, ZCL_FRAME_CLIENT_SERVER_DIR, (d), 0, (e), 2, (c) )
    
    
    
    void zclSampleSw_actionToggleLight(const int32_t _itemEntry)
    {
        zstack_getZCLFrameCounterRsp_t Rsp;
    
        Zstackapi_getZCLFrameCounterReq(appServiceTaskId, &Rsp);
        zclSampleSw_DstAddr.addrMode = afAddr16Bit;
        zclSampleSw_DstAddr.addr.shortAddr = 0xe0c1;
        zclSampleSw_DstAddr.endPoint = 8;
        zclSampleSw_DstAddr.panId = 0xd02a;
        zclGeneral_SendOnOff_CmdOnDuration( SAMPLESW_ENDPOINT, &zclSampleSw_DstAddr, 0, TRUE, Rsp.zclFrameCounter);
    }

    实验现象:

    1.发送的数据,终端能触发zstackmsg_CmdIDs_AF_INCOMING_MSG_IND,说明有数据过来

    2.但是 zclonDurationCB 这个callback没有执行,不知道什么原因

  • 設置個斷點在zclGeneral_ProcessInOnOff裡頭,看看會不會進去
  • static ZStatus_t zclGeneral_ProcessInOnOff( zclIncoming_t *pInMsg,
                                                zclGeneral_AppCallbacks_t *pCBs )
    {
      ZStatus_t stat = ZSuccess;
    
      if ( zcl_ServerCmd( pInMsg->hdr.fc.direction ) )
      {
        switch ( pInMsg->hdr.commandID )
        {
          case COMMAND_ON_OFF_OFF:
          case COMMAND_ON_OFF_ON:
          case COMMAND_ON_OFF_TOGGLE:
            if ( pCBs->pfnOnOff )
            {
              pCBs->pfnOnOff( pInMsg->hdr.commandID );
            }
            break;
    
    #ifdef ZCL_LIGHT_LINK_ENHANCE
          case COMMAND_ON_OFF_OFF_WITH_EFFECT:
            if ( pCBs->pfnOnOff_OffWithEffect )
            {
              zclOffWithEffect_t cmd;
    
              cmd.srcAddr = &(pInMsg->msg->srcAddr);
              cmd.effectId = pInMsg->pData[0];
              cmd.effectVariant = pInMsg->pData[1];
    
              pCBs->pfnOnOff_OffWithEffect( &cmd );
            }
            break;
    
          case COMMAND_ON_OFF_ON_WITH_RECALL_GLOBAL_SCENE:
            if ( pCBs->pfnOnOff_OnWithRecallGlobalScene )
            {
              pCBs->pfnOnOff_OnWithRecallGlobalScene();
            }
            break;
    
          case COMMAND_ON_OFF_ON_WITH_TIMED_OFF:
            if ( pCBs->pfnOnOff_OnWithTimedOff )
            {
              zclOnWithTimedOff_t cmd;
    
              cmd.onOffCtrl.byte = pInMsg->pData[0];
              cmd.onTime = BUILD_UINT16( pInMsg->pData[1], pInMsg->pData[2] );
              cmd.offWaitTime = BUILD_UINT16( pInMsg->pData[3], pInMsg->pData[4] );
              pCBs->pfnOnOff_OnWithTimedOff( &cmd );
            }
            break;
    #endif // ZCL_LIGHT_LINK_ENHANCE
    
          default:
            stat = ZFailure;
            break;
        }
      }
      // no Client command
    
      return ( stat );
    }

    问题找到了,由于ZCL_LIGHT_LINK_ENHANCE这个没有定义 ,所以导致case COMMAND_ON_OFF_ON_WITH_TIMED_OFF:一直没有被触发。

    ZCL_LIGHT_LINK_ENHANCE这个定义是什么意思?我如果define这个定义会有什么影响吗??

    多谢

  • 這些command一開始是從Zigbee Light Link開始的,所以才有ZCL_LIGHT_LINK_ENHANCE这个定义,基本上要能支援基本的ON/OFF command 之外,就是要加上这个定义