Other Parts Discussed in Thread: Z-STACK
查了许多资料,发现TI zstack 进入睡眠好像没有完整的案例,特别是低功耗,非常零散,现在电流有300uA,都不知道有没有进入低功耗,外部有两个按钮采用上拉电阻,中断触发方式,一个LED 灯,LED 灯是高电平驱动点亮,求教,按照他们说的编译选项,都做了,
NWK_AUTO_POLL
xZTOOL_P1
xMT_TASK
xMT_SYS_FUNC
xMT_ZDO_FUNC
xLCD_SUPPORTED=DEBUG
POWER_SAVING
xNV_RESTORE
xNV_INIT
xHOLD_AUTO_START
/****************************************
* The following are for End Devices only
***************************************/
-DRFD_RCVC_ALWAYS_ON=FALSE
/* The number of milliseconds to wait between data request polls to the coordinator. */
-DPOLL_RATE=0
/* This is used after receiving a data indication to poll immediately
* for queued messages...in milliseconds.
*/
-DQUEUED_POLL_RATE=0
/* This is used after receiving a data confirmation to poll immediately
* for response messages...in milliseconds
*/
-DRESPONSE_POLL_RATE=0
/* This is used as an alternate response poll rate only for rejoin request.
* This rate is determined by the response time of the parent that the device
* is trying to join.
*/
-DREJOIN_POLL_RATE=440
void osal_pwrmgr_init( void )
{
pwrmgr_attribute.pwrmgr_device =PWRMGR_BATTERY; // Default to no power conservation.
pwrmgr_attribute.pwrmgr_task_state = 0; // Cleared. All set to conserve
}
没有osal_start_timeEX 事件,
两个按键P00 P01 都是下降沿触发中断,
/* Enable/Disable Interrupt or */
Hal_KeyIntEnable = interruptEnable;
/* Register the callback fucntion */
pHalKeyProcessFunction = cback;
/* Determine if interrupt is enable or not */
//Rising/Falling edge configuratinn */
IEN1|=0x20;//开启P0端口中断
P0IEN|=0x03;
magneticSensorLastState=HAL_KEY_SW_OFF;
PICTL &= ~(HAL_KEY_SW_1_EDGEBIT); /* Clear the edge bit */
/* For falling edge, the bit must be set. */
/*#if (HAL_KEY_SW_1_EDGE == HAL_KEY_FALLING_EDGE)
PICTL |= HAL_KEY_SW_1_EDGEBIT;--//产生中断
#endif*/
//传感器接口
PICTL &= ~(HAL_KEY_SW_2_EDGEBIT); /* Clear the edge bit */
/* For falling edge, the bit must be set. */
/* #if (HAL_KEY_SW_2_EDGE == HAL_KEY_FALLING_EDGE)
PICTL |= HAL_KEY_SW_2_EDGEBIT;//产生中断
#endif*/
/* Interrupt configuration:
* - Enable interrupt generation at the port
* - Enable CPU interrupt
* - Clear any pending interrupt
*/
HAL_KEY_SW_1_ICTL |= HAL_KEY_SW_1_ICTLBIT;
HAL_KEY_SW_1_IEN |= HAL_KEY_SW_1_IENBIT;
HAL_KEY_SW_1_PXIFG = ~(HAL_KEY_SW_1_BIT);
//传感器接口
HAL_KEY_SW_2_ICTL |= HAL_KEY_SW_2_ICTLBIT;
HAL_KEY_SW_2_IEN |= HAL_KEY_SW_2_IENBIT;
HAL_KEY_SW_2_PXIFG = ~(HAL_KEY_SW_2_BIT);
P0INP&=~(1<<0); // P0_0定义为上下拉模式
P0INP&=~(1<<1); // P0_1定义为上下拉模式
P2INP&=~(1<<5); //上拉
/* Interrupt configuration:
* - Enable interrupt generation at the port
* - Enable CPU interrupt
* - Clear any pending interrupt
*/
/* Do this only after the hal_key is configured - to work with sleep stuff */
if (HalKeyConfigured == TRUE)
{
osal_stop_timerEx( Hal_TaskID, HAL_KEY_EVENT); /* Cancel polling if active */
}
/* Key now is configured */
HalKeyConfigured = TRUE;
不知道电流怎么一直在300uA左右,