Part Number: CC2530
zigbee mesh组网 怎样读出路由节点的收包数量?或者是转发包的数量。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
网上有个前辈说,在代码收到并处理无线数据的地方开个计数器,每次运行到这里就加1,这个方法行得通吗?
您好,我把代码加在黄色背景部分(两处均试过),来统计收包数量 h ,发现随着路由节点的子节点数量增加,路由节点的 h 的增加速率并没有改变,这是为什么?问题出在哪?以下为部分代码。感谢解答
uint16 i = 0;
uint16 SampleApp_ProcessEvent( uint8 task_id, uint16 events )
{
uint8 Display_Buf[6] = {0};
uint16 shortAddr = 0;
uint16 shortAddrNew = 0;
uint16 PANID=0;
uint16 parentshortAddr = 0;
uint16 parentshortAddrNew = 0;
uint16 h;
afIncomingMSGPacket_t *MSGpkt;
(void)task_id; // Intentionally unreferenced parameter
if ( events & SYS_EVENT_MSG ) /*系统消息事件*/
{
h=i;
num_to_str(h, Display_Buf, 4 , 16);
Gui_DrawFont_GBK16(0,96,BLACK,YELLOW,Display_Buf);
i++;
MSGpkt = (afIncomingMSGPacket_t *)osal_msg_receive( SampleApp_TaskID );
while ( MSGpkt ) /*调用数据接收函数接收数据.2*/
{
switch ( MSGpkt->hdr.event ) /*判断具体事件*/
{
// Received when a key is pressed
case KEY_CHANGE:
SampleApp_HandleKeys( ((keyChange_t *)MSGpkt)->state, ((keyChange_t *)MSGpkt)->keys );
break; /*如果为按键事件,调用案件处理函数.3*/
// Received when a messages is received (OTA) for this endpoint
case AF_INCOMING_MSG_CMD:
HAL_TOGGLE_LED1(); /*?*/
SampleApp_MessageMSGCB( MSGpkt );
// h=i;
// num_to_str(h,Display_Buf, 4 , 16);
// Gui_DrawFont_GBK16(0,96,BLACK,YELLOW,Display_Buf);
// i++;
break; /*如果为数据接收事件,调用数据接收函数.3*/
// Received whenever the device changes state in the network
case ZDO_STATE_CHANGE:
SampleApp_NwkState = (devStates_t)(MSGpkt->hdr.status);
if ( (SampleApp_NwkState == DEV_ZB_COORD)
||(SampleApp_NwkState == DEV_ROUTER)
|| (SampleApp_NwkState == DEV_END_DEVICE) ) /*如果为网络状态改变事件,则判断网络类型.5*/
{
if(SampleApp_NwkState == DEV_END_DEVICE)
{
Gui_DrawFont_GBK16(0,16,RED,CYAN," EndDevice ");
Gui_DrawFont_GBK16(0,48,BLACK,YELLOW,"ShortAddr: ");
Gui_DrawFont_GBK16(0,64,BLACK,YELLOW, "Temp:");
Gui_DrawFont_GBK16(0,80,BLACK,YELLOW, "parentSA:");
}
else if(SampleApp_NwkState == DEV_ZB_COORD)
{
Gui_DrawFont_GBK16(0,16,RED,CYAN," CooDevice ");
}
else
{
Gui_DrawFont_GBK16(0,16,RED,CYAN," RouterDevice ");
Gui_DrawFont_GBK16(0,48,BLACK,YELLOW,"ShortAddr: ");
Gui_DrawFont_GBK16(0,64,BLACK,YELLOW, "parentSA:");
}
if ( (SampleApp_NwkState == DEV_ROUTER)
|| (SampleApp_NwkState == DEV_END_DEVICE) )
{
//显示设备地址shortAddr
zb_GetDeviceInfo(ZB_INFO_SHORT_ADDR, &shortAddr);
shortAddrNew = LO_UINT16(shortAddr) << 8;
shortAddrNew = HI_UINT16(shortAddr) |shortAddrNew;
num_to_str(shortAddrNew, Display_Buf, 4 , 16);
Gui_DrawFont_GBK16(94,48,BLACK,YELLOW,Display_Buf);
//显示父节点
zb_GetDeviceInfo(ZB_INFO_PARENT_SHORT_ADDR, &parentshortAddr);
parentshortAddrNew = LO_UINT16(parentshortAddr) << 8;
parentshortAddrNew = HI_UINT16(parentshortAddr) |parentshortAddrNew;
num_to_str(parentshortAddrNew, Display_Buf, 4 , 16);
Gui_DrawFont_GBK16(94,80,BLACK,YELLOW,Display_Buf);
// Start sending the periodic message in a regular interval.
osal_start_timerEx( SampleApp_TaskID,
SAMPLEAPP_SEND_PERIODIC_MSG_EVT,
SAMPLEAPP_SEND_PERIODIC_MSG_TIMEOUT ); /*调用定时函数,进行定时事件处理.3*/
}
//显示PANID
zb_GetDeviceInfo(ZB_INFO_PAN_ID, &PANID);
num_to_str(PANID, Display_Buf, 4 , 16);
Gui_DrawFont_GBK16(94,32,BLACK,YELLOW,Display_Buf);
}
else
{
// Device is no longer in the network
}
break;
default:
break;
}
// Release the memory
osal_msg_deallocate( (uint8 *)MSGpkt ); /*释放空间*/
// Next - if one is available
MSGpkt = (afIncomingMSGPacket_t *)osal_msg_receive( SampleApp_TaskID ); /*调用数据接收函数接收数据*/
h=i;
num_to_str(h,Display_Buf, 4 , 16);
Gui_DrawFont_GBK16(0,96,BLACK,YELLOW,Display_Buf);
i++;
}
// return unprocessed events返回未处理的事件
return (events ^ SYS_EVENT_MSG);
}
// Send a message out - This event is generated by a timer发送消息-此事件由计时器生成
// (setup in SampleApp_Init()).
if ( events & SAMPLEAPP_SEND_PERIODIC_MSG_EVT ) /*如果为定时事件,进行定时事件处理*/
{
// Send the periodic message
// SampleApp_SendPeriodicMessage();
// HalUARTWrite(0,"UartInit OK\n", sizeof("UartInit OK\n"));//提示信息
if(SampleApp_NwkState == DEV_ROUTER)
{
//sendDummyReport();
sendReport();
osal_start_timerEx( SampleApp_TaskID, SAMPLEAPP_SEND_PERIODIC_MSG_EVT,
(SAMPLEAPP_SEND_PERIODIC_MSG_TIMEOUT + (osal_rand() & 0x00FF)) ); /*循环调用定时函数.2*/
}
else{
DHT11_TEST();
sendReport();
num_to_str(ucharT_data_H, Display_Buf, 4 , 10 );
Gui_DrawFont_GBK16(94,64,BLACK,YELLOW, Display_Buf);
// Setup to send message again in normal period (+ a little jitter)
osal_start_timerEx( SampleApp_TaskID, SAMPLEAPP_SEND_PERIODIC_MSG_EVT,
(SAMPLEAPP_SEND_PERIODIC_MSG_TIMEOUT + (osal_rand() & 0x00FF)) ); /*循环调用定时函数.2*/
// HAL_TOGGLE_LED1();
// HAL_TOGGLE_LED2();
}
// return unprocessed events
return (events ^ SAMPLEAPP_SEND_PERIODIC_MSG_EVT);
}
// Discard unknown events
return 0;
}