Part Number: CC2530
现在有一个变量 h,我想计算每分钟 h 增加的数量,用什么可以实现每分钟使 h 清零重新计数?有简单的方法吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我加上去并没有实现,不知道错在哪,我需要把变量n定时清零,重新计数(黄色背景部分)。
uint16 SampleApp_ProcessEvent( uint8 task_id, uint16 events )
{
uint8 Display_Buf[6] = {0};
uint16 shortAddr = 0;
uint16 shortAddrNew = 0;
uint16 PANID=0;
uint16 parentshortAddr = 0;
uint16 parentshortAddrNew = 0;
// uint16 h;
afIncomingMSGPacket_t *MSGpkt;
(void)task_id; // Intentionally unreferenced parameter
if ( events & SYS_EVENT_MSG ) /*系统消息事件*/
{
MSGpkt = (afIncomingMSGPacket_t *)osal_msg_receive( SampleApp_TaskID );
while ( MSGpkt ) /*调用数据接收函数接收数据.2*/
{
switch ( MSGpkt->hdr.event ) /*判断具体事件*/
{
// Received when a key is pressed
case KEY_CHANGE:
SampleApp_HandleKeys( ((keyChange_t *)MSGpkt)->state, ((keyChange_t *)MSGpkt)->keys );
break; /*如果为按键事件,调用案件处理函数.3*/
// Received when a messages is received (OTA) for this endpoint
case AF_INCOMING_MSG_CMD:
HAL_TOGGLE_LED1(); /*?*/
SampleApp_MessageMSGCB( MSGpkt );
n=n+1;
m=n;
osal_start_timerEx(SampleApp_TaskID,CLEAR_EVT,CLEAR_EVENT_TIMEOUT);
num_to_str(m,Display_Buf, 4 , 16);
Gui_DrawFont_GBK16(48,96,BLACK,YELLOW,Display_Buf);
if (m>0x20)
{
void leaveNetBySelf(void);
{
NLME_LeaveReq_t leaveReq;
osal_memset((uint8 *)&leaveReq,0,sizeof(NLME_LeaveReq_t));
osal_memcpy(leaveReq.extAddr,NLME_GetExtAddr(),Z_EXTADDR_LEN);
// zgWriteStartupOptions(ZG_STARTUP_SET, ZCD_STARTOPT_DEFAULT_NETWORK_STATE);
// SystemReset();
leaveReq.removeChildren = 1;
leaveReq.rejoin = 0;
leaveReq.silent = 0;
Delay_3000us();
SystemReset();
// osal_start_timerEx(SampleApp_TaskID,SAMPLEAPP_SEND_PERIODIC_MSG_EVT,15000); //使m定时清零
// m=0;
// HalLedBlink (HAL_LED_1, 0, 50, 2000 );
// if( NLME_LeaveReq(&leaveReq)!=afStatus_SUCCESS )
// {
// ZDApp_LeaveReset(false);
// }
}
}
break; /*如果为数据接收事件,调用数据接收函数.3*/
if ( events & CLEAR_EVT )
{ n=0;
osal_start_timerEx(SampleApp_TaskID,CLEAR_EVT,CLEAR_EVENT_TIMEOUT);
return (events & CLEAR_EVT);
}
你在每次收到AF_INCOMING_MSG_CMD 就調用osal_start_timerEx去啟動CLEAR_EVENT_TIMEOUT應該不大對吧,不是應該在init的時候調用?
我加入到这里,发现清零后计数到1,就一直不变了,这是哪里的问题,(相关代码黄色背景部分)谢前辈解答
void SampleApp_Init( uint8 task_id )
{
//点对点通信
Point_To_Point_DstAddr.addrMode=(afAddrMode_t)Addr16Bit;
Point_To_Point_DstAddr.endPoint=SAMPLEAPP_ENDPOINT;
Point_To_Point_DstAddr.addr.shortAddr=0x0000;
SampleApp_TaskID = task_id; /*任务ID*/
SampleApp_NwkState = DEV_INIT; /*网络状态*/
SampleApp_TransID = 0; /*传输序列号*/
uint8 Display_Buf[6] = {0};
halUARTCfg_t uartConfig;
// MT_UartInit(); //串口初始化
uartConfig.configured = TRUE; // 2x30 don't care - see uart driver.
uartConfig.baudRate = HAL_UART_BR_38400;
uartConfig.flowControl = FALSE;
uartConfig.flowControlThreshold = 48; // 2x30 don't care - see uart driver.
uartConfig.rx.maxBufSize = 128; // 2x30 don't care - see uart driver.
uartConfig.tx.maxBufSize = 128; // 2x30 don't care - see uart driver.
uartConfig.idleTimeout = 6; // 2x30 don't care - see uart driver.
uartConfig.intEnable = TRUE; // 2x30 don't care - see uart driver.
uartConfig.callBackFunc = uartRxCB;
HalUARTOpen (0, &uartConfig);
MT_UartRegisterTaskID(task_id); //注册串口任务
// HalUARTWrite(0,"UartInit OK\n", sizeof("UartInit OK\n"));//提示信息
// Device hardware initialization can be added here or in main() (Zmain.c).
// If the hardware is application specific - add it here.
// If the hardware is other parts of the device add it in main().
dsp_single_colour(YELLOW);
Line_Dsp_single_colour(0,0,128,32,CYAN);
//向lcd输出相关信息
Gui_DrawFont_GBK16(0,0,RED,CYAN, " ZigBee topology ");
Gui_DrawFont_GBK16(0,32,BLACK,YELLOW,"Panid: ");
#if defined ( BUILD_ALL_DEVICES )
// The "Demo" target is setup to have BUILD_ALL_DEVICES and HOLD_AUTO_START
// We are looking at a jumper (defined in SampleAppHw.c) to be jumpered
// together - if they are - we will start up a coordinator. Otherwise,
// the device will start as a router.
if ( readCoordinatorJumper() )
zgDeviceLogicalType = ZG_DEVICETYPE_COORDINATOR;
else
zgDeviceLogicalType = ZG_DEVICETYPE_ROUTER;
#endif // BUILD_ALL_DEVICES
#if defined ( HOLD_AUTO_START ) /*ZDO初始化*/
HOLD_AUTO_START is a compile option that will surpress ZDApp
from starting the device and wait for the application to
start the device.
ZDOInitDevice(0);
#endif
// Setup for the periodic message's destination address
// Broadcast to everyone
SampleApp_Periodic_DstAddr.addrMode = (afAddrMode_t)Addr16Bit;
SampleApp_Periodic_DstAddr.endPoint = SAMPLEAPP_ENDPOINT;
SampleApp_Periodic_DstAddr.addr.shortAddr = 0x0000; /*以上三行为数据广播地址初始化*/
// Setup for the flash command's destination address - Group 1
SampleApp_Flash_DstAddr.addrMode = (afAddrMode_t)afAddrGroup;
SampleApp_Flash_DstAddr.endPoint = SAMPLEAPP_ENDPOINT;
SampleApp_Flash_DstAddr.addr.shortAddr = SAMPLEAPP_FLASH_GROUP; /*以上三行为组播地址初始化*/
// Fill out the endpoint description.
SampleApp_epDesc.endPoint = SAMPLEAPP_ENDPOINT;
SampleApp_epDesc.task_id = &SampleApp_TaskID;
SampleApp_epDesc.simpleDesc
= (SimpleDescriptionFormat_t *)&SampleApp_SimpleDesc;
SampleApp_epDesc.latencyReq = noLatencyReqs; /*以上为端点信息初始化*/
// Register the endpoint description with the AF
afRegister( &SampleApp_epDesc ); /*注册端点至AF层*/
// Register for all key events - This app will handle all key events
RegisterForKeys( SampleApp_TaskID ); /*注册按键*/
// By default, all devices start out in Group 1
SampleApp_Group.ID = 0x0001;
osal_memcpy( SampleApp_Group.name, "Group 1", 7 ); /*组名设置为group 1*/
aps_AddGroup( SAMPLEAPP_ENDPOINT, &SampleApp_Group ); /*将组信息添加至aps层*/ /*组信息初始化.3*/
osal_start_timerEx(SampleApp_TaskID,CLEAR_EVT,CLEAR_EVENT_TIMEOUT);
#if defined ( LCD_SUPPORTED )
HalLcdWriteString( "SampleApp", HAL_LCD_LINE_1 );
#endif
}
void Delay_3000us(void) //10 us延时
{
MicroWait(3000);
}
/*如果定义了LCD,LCD显示.4*/
/*********************************************************************
* @fn SampleApp_ProcessEvent
*
* @brief Generic Application Task event processor. This function
* is called to process all events for the task. Events
* include timers, messages and any other user defined events.
*
* @param task_id - The OSAL assigned task ID.
* @param events - events to process. This is a bit map and can
* contain more than one event.
*
* @return none
*/
uint16 i = 0;
uint16 h;
uint16 j = 0;
uint16 s;
uint16 n = 0;
uint16 m;
uint16 SampleApp_ProcessEvent( uint8 task_id, uint16 events )
{
uint8 Display_Buf[6] = {0};
uint16 shortAddr = 0;
uint16 shortAddrNew = 0;
uint16 PANID=0;
uint16 parentshortAddr = 0;
uint16 parentshortAddrNew = 0;
// uint16 h;
afIncomingMSGPacket_t *MSGpkt;
(void)task_id; // Intentionally unreferenced parameter
if ( events & SYS_EVENT_MSG ) /*系统消息事件*/
{
MSGpkt = (afIncomingMSGPacket_t *)osal_msg_receive( SampleApp_TaskID );
while ( MSGpkt ) /*调用数据接收函数接收数据.2*/
{
switch ( MSGpkt->hdr.event ) /*判断具体事件*/
{
// Received when a key is pressed
case KEY_CHANGE:
SampleApp_HandleKeys( ((keyChange_t *)MSGpkt)->state, ((keyChange_t *)MSGpkt)->keys );
break; /*如果为按键事件,调用案件处理函数.3*/
// Received when a messages is received (OTA) for this endpoint
case AF_INCOMING_MSG_CMD:
HAL_TOGGLE_LED1(); /*?*/
SampleApp_MessageMSGCB( MSGpkt );
n=n+1;
m=n;
num_to_str(m,Display_Buf, 4 , 16);
Gui_DrawFont_GBK16(48,96,BLACK,YELLOW,Display_Buf);
if (m>0x20)
{
void leaveNetBySelf(void);
{
NLME_LeaveReq_t leaveReq;
osal_memset((uint8 *)&leaveReq,0,sizeof(NLME_LeaveReq_t));
osal_memcpy(leaveReq.extAddr,NLME_GetExtAddr(),Z_EXTADDR_LEN);
// zgWriteStartupOptions(ZG_STARTUP_SET, ZCD_STARTOPT_DEFAULT_NETWORK_STATE);
// SystemReset();
leaveReq.removeChildren = 1;
leaveReq.rejoin = 0;
leaveReq.silent = 0;
Delay_3000us();
SystemReset();
}
}
break; /*如果为数据接收事件,调用数据接收函数.3*/
// Received whenever the device changes state in the network
case ZDO_STATE_CHANGE:
if(SampleApp_NwkState == DEV_NWK_ORPHAN)
{
void leaveNetBySelf(void);
{
//主动离开参考
NLME_LeaveReq_t leaveReq;
osal_memset((uint8 *)&leaveReq,0,sizeof(NLME_LeaveReq_t));
osal_memcpy(leaveReq.extAddr,NLME_GetExtAddr(),Z_EXTADDR_LEN);
// zgWriteStartupOptions(ZG_STARTUP_SET, ZCD_STARTOPT_DEFAULT_NETWORK_STATE);
// SystemReset();
leaveReq.removeChildren = 1;
leaveReq.rejoin = 0;
leaveReq.silent = 0;
SystemReset();
// HalLedBlink (HAL_LED_1, 0, 50, 2000 );
// if( NLME_LeaveReq(&leaveReq)!=afStatus_SUCCESS )
// {
// ZDApp_LeaveReset(false);
// }
}
}
SampleApp_NwkState = (devStates_t)(MSGpkt->hdr.status);
if ( (SampleApp_NwkState == DEV_ZB_COORD)
||(SampleApp_NwkState == DEV_ROUTER)
|| (SampleApp_NwkState == DEV_END_DEVICE) ) /*如果为网络状态改变事件,则判断网络类型.5*/
{
// osal_start_timerEx(SampleApp_TaskID,CLEAR_EVT,15000);
if(SampleApp_NwkState == DEV_END_DEVICE)
{
Gui_DrawFont_GBK16(0,16,RED,CYAN," EndDevice ");
Gui_DrawFont_GBK16(0,48,BLACK,YELLOW,"ShortAddr: ");
Gui_DrawFont_GBK16(0,64,BLACK,YELLOW, "Temp:");
Gui_DrawFont_GBK16(0,80,BLACK,YELLOW, "parentSA:");
}
else if(SampleApp_NwkState == DEV_ZB_COORD)
{
Gui_DrawFont_GBK16(0,16,RED,CYAN," CooDevice ");
}
else
{
Gui_DrawFont_GBK16(0,16,RED,CYAN," RouterDevice ");
Gui_DrawFont_GBK16(0,48,BLACK,YELLOW,"ShortAddr: ");
Gui_DrawFont_GBK16(0,64,BLACK,YELLOW, "parentSA:");
}
if ( (SampleApp_NwkState == DEV_ROUTER)
|| (SampleApp_NwkState == DEV_END_DEVICE) )
{
//显示设备地址shortAddr
zb_GetDeviceInfo(ZB_INFO_SHORT_ADDR, &shortAddr);
shortAddrNew = LO_UINT16(shortAddr) << 8;
shortAddrNew = HI_UINT16(shortAddr) |shortAddrNew;
num_to_str(shortAddrNew, Display_Buf, 4 , 16);
Gui_DrawFont_GBK16(94,48,BLACK,YELLOW,Display_Buf);
//显示父节点
zb_GetDeviceInfo(ZB_INFO_PARENT_SHORT_ADDR, &parentshortAddr);
parentshortAddrNew = LO_UINT16(parentshortAddr) << 8;
parentshortAddrNew = HI_UINT16(parentshortAddr) |parentshortAddrNew;
num_to_str(parentshortAddrNew, Display_Buf, 4 , 16);
Gui_DrawFont_GBK16(94,80,BLACK,YELLOW,Display_Buf);
// Start sending the periodic message in a regular interval.
osal_start_timerEx( SampleApp_TaskID,
SAMPLEAPP_SEND_PERIODIC_MSG_EVT,
SAMPLEAPP_SEND_PERIODIC_MSG_TIMEOUT ); /*调用定时函数,进行定时事件处理.3*/
}
//显示PANID
zb_GetDeviceInfo(ZB_INFO_PAN_ID, &PANID);
num_to_str(PANID, Display_Buf, 4 , 16);
Gui_DrawFont_GBK16(94,32,BLACK,YELLOW,Display_Buf);
}
else
{
// Device is no longer in the network
}
break;
default:
break;
}
// Release the memory
osal_msg_deallocate( (uint8 *)MSGpkt ); /*释放空间*/
// Next - if one is available
MSGpkt = (afIncomingMSGPacket_t *)osal_msg_receive( SampleApp_TaskID ); /*调用数据接收函数接收数据*/
//以下勿删
// h=i;
// num_to_str(h,Display_Buf, 4 , 16);
// Gui_DrawFont_GBK16(0,96,BLACK,YELLOW,Display_Buf);
// i++;
// void leaveNetBySelf(void);
// {
// if ( h>0x010)
// {
// //主动离开参考
// NLME_LeaveReq_t leaveReq;
// osal_memset((uint8 *)&leaveReq,0,sizeof(NLME_LeaveReq_t));
// osal_memcpy(leaveReq.extAddr,NLME_GetExtAddr(),Z_EXTADDR_LEN);
//// zgWriteStartupOptions(ZG_STARTUP_SET, ZCD_STARTOPT_DEFAULT_NETWORK_STATE);
//// SystemReset();
// leaveReq.removeChildren = 1;
// leaveReq.rejoin = 0;
// leaveReq.silent = 0;
// SystemReset();
//// HalLedBlink (HAL_LED_1, 0, 50, 2000 );
// if( NLME_LeaveReq(&leaveReq)!=afStatus_SUCCESS )
// {
//
//
// ZDApp_LeaveReset(false);
// }
// }
// }
}
// return unprocessed events返回未处理的事件
return (events ^ SYS_EVENT_MSG);
}
if ( events & CLEAR_EVT )
{ n=0;
osal_start_timerEx(SampleApp_TaskID,CLEAR_EVT,CLEAR_EVENT_TIMEOUT);
return (events & CLEAR_EVT);
}
// Send a message out - This event is generated by a timer发送消息-此事件由计时器生成
// (setup in SampleApp_Init()).
if ( events & SAMPLEAPP_SEND_PERIODIC_MSG_EVT ) /*如果为定时事件,进行定时事件处理*/
{
// Send the periodic message
// SampleApp_SendPeriodicMessage();
// HalUARTWrite(0,"UartInit OK\n", sizeof("UartInit OK\n"));//提示信息
if(SampleApp_NwkState == DEV_ROUTER)
{
//sendDummyReport();
sendReport();
osal_start_timerEx( SampleApp_TaskID, SAMPLEAPP_SEND_PERIODIC_MSG_EVT,
(SAMPLEAPP_SEND_PERIODIC_MSG_TIMEOUT + (osal_rand() & 0x00FF)) ); /*循环调用定时函数.2*/
}
else{
DHT11_TEST();
sendReport();
num_to_str(ucharT_data_H, Display_Buf, 4 , 10 );
Gui_DrawFont_GBK16(94,64,BLACK,YELLOW, Display_Buf);
// Setup to send message again in normal period (+ a little jitter)
osal_start_timerEx( SampleApp_TaskID, SAMPLEAPP_SEND_PERIODIC_MSG_EVT,
(SAMPLEAPP_SEND_PERIODIC_MSG_TIMEOUT + (osal_rand() & 0x00FF)) ); /*循环调用定时函数.2*/
// HAL_TOGGLE_LED1();
// HAL_TOGGLE_LED2();
}
// return unprocessed events
return (events ^ SAMPLEAPP_SEND_PERIODIC_MSG_EVT);
}
// Discard unknown events
return 0;
}
你return (events & CLEAR_EVT);應該要改成return (events ^ CLEAR_EVT);
你應該調試看看是不是沒有AF_INCOMING_MSG_CMD導致沒有繼續累加,另外你的CLEAR_EVENT_TIMEOUT是多大?
1. 調試看看是不是沒有AF_INCOMING_MSG_CMD導致沒有繼續累加
2. 調試看看CLEAR_EVENT是不是50秒被觸發一次,還是一直被觸發,另外,你CLEAR_EVENT的定義是?
调试我不太会,我再学学,好像一直在循环CLEAR_EVENT,这个该怎么定义?除了.C文件中的那些代码,还需要其他的定义吗?
#define CLEAR_EVT 0x0002
一直在循环CLEAR_EVENT你可能要查一下是不是有其他的事件也定義為0x0002了
1、我经过调试发现,运行到 n=0,会在此一直循环运行这一句,有时会跳出来运行一次 n+1,但下一步又会回到 n=0 .
2、事件号我也改过,还是不行。
解决了解决了,我是代码有些错误,我太马虎了,多谢大佬指点,您是我的榜样!!!