This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: 和CC2652RB运行zigbee协议栈有什么区别?

Part Number: CC2652R

1. CC2652RB无需外部晶振可以运行zigbee协议栈?

2. CC2652R的zigbee工程能如何替换为CC2652RB的工程?

3. CC2652R和CC2652RB哪种更适合稳定运行zigbee协议栈?

  • 如果是同一版本的SDK,协议栈则是相同的,没有区别,唯一不同的是硬件引起的差别

    1.可以,C2652RB 具有一个集成式 BAW(体声波)谐振器,用于产生射频载波,因此无需使用外部 48MHz 晶体

    2.将应用部分移植到CC2652RB工程中即可

    3.都可以,没有太大差别,使用CC2652RB的好处是可以节省PCB空间,因为它没有外部晶振