Part Number: CC2530
在Zstack 2.5.1a中,Coordinator节点使用AF_DataRequest发送一组十六进制数据uint8 theMessageData[128] = {0x02, 0x03, 0x10, 0x00, 0x35, 0x00, 0xF2, 0x00};
使用EndDevice接收,但收到的数据只有{02 03 10},请问为什么会出现这样的问题?如何解决?

主要代码如下:
//按键按下事件,自定义
if ( events & X1_KEY_EVT )
{
GenericApp_SendTheMessage(); //发送Hello World
HalUARTWrite(0, "The Key is down\n", sizeof("The Key is down\n"));
HalLedSet(HAL_LED_1, HAL_LED_MODE_TOGGLE);
return (events ^ X1_KEY_EVT);
}
static void GenericApp_SendTheMessage( void )
{
// char theMessageData[] = "Hello World!\n";
uint8 theMessageData[128] = {0x02, 0x03, 0x10, 0x00, 0x35, 0x00, 0xF2, 0x00};
AF_DataRequest( &GenericApp_DstAddr, &GenericApp_epDesc,
GENERICAPP_CLUSTERID,
(byte)osal_strlen( theMessageData ) + 1,
(byte *)&theMessageData,
&GenericApp_TransID,
AF_DISCV_ROUTE, AF_DEFAULT_RADIUS );
}
//终端节点接收
static void GenericApp_MessageMSGCB( afIncomingMSGPacket_t *pkt )
{
uint8 buffer[20];
switch ( pkt->clusterId )
{
case GENERICAPP_CLUSTERID:
osal_memcpy(buffer, pkt->cmd.Data, osal_strlen((char *)pkt->cmd.Data));
HalUARTWrite(0, buffer, osal_strlen((char *)pkt->cmd.Data));
break;
}
}