This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: CC2530 debug功能

Part Number: CC2530


您好:我们正在使用CC2530F256RHAT,想要增加debug烧写功能;查看资料发现IC管脚P2_2、P2_1分别为Debug_CLK、Debug_DATA;问题如下:

1. 只需要引出Debug_CLK、Debug_DATA、GND 这三根数据线,就能够实现debug功能吗?

2. Debug_CLK、Debug_DATA与 reset 存在什么关系? 我现在是将CC2530做成一个小板(小板上预留USB接口),插接在主板上;通过主板控制CC2530复位;若将小板与主板分离,单独调测小板(CC2530),即CC2530无主板初始化复位控制,该怎样能实现debug功能呢?