This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2531EMK: 如何在基于ARM64架构的windows11系统中安装usb dongle CC2531的驱动啊?

Part Number: CC2531EMK
Other Parts Discussed in Thread: CC2531,

在windows系统CPU为X86/X64安装驱动是正常的,但在ARM64位的系统中安装不成功,个人感觉可能是驱动的问题,哪里能下载ARM64位的windows11的cc2531 usb dongle 的驱动??

  • 您好,

    我们还是建议您选择X86/X64的电脑进行操作。

    根据CC2531EMK Quick Start Guide,链接,和SmartRFTm Packet Sniffer User's Manual ,链接。

    有提到:

    The following operating systems are supported:

    •  Windows XP/Pro (32 bit)
    •  Windows Vista (32 bit)
    •  Windows Vista (64 bit)
    •  Windows 7 (32 bit)
    •  Windows 7 (64 bit)
    •  Windows 8 (64 bit)

    没有提到有对Windows on ARM的支持。

    感谢您的支持,希望能够帮助到您。