Part Number: CC2530
CC2530先设置为上升沿捕获,进入上升沿捕获中断后,设置为下降沿捕获,以此来测得高电平的时间。但是在使用的时候发现,只有调试的过程中才能进入上升沿中断当中去,而无法进入下降沿中断。具体代码如下:
/****************************************************************************
* 文 件 名: main.c
* 作 者: Andy
* 修 订: 2013-01-08
* 版 本: 1.0
* 描 述: 定时器T3通过中断方式控制LED1周期性闪烁
****************************************************************************/
#include <ioCC2530.h>
typedef unsigned char uchar;
typedef unsigned int uint;
unsigned char irtime=0;
#define IR P1_0
#define uint32_t unsigned int
#define uint16_t unsigned short
#define uint8_t unsigned char
unsigned char receive_ok=1;
uint32_t upCount=0;
uint16_t valueDown=0;
uint16_t valueUp=0;
uint32_t width=0;
uint32_t isUpCap=1;
uint buffer[200]={0};
char bufferId=0;
//#define leng_23
//#define leng_21
#if defined leng_23
uint8_t leng=23;
uint8_t arr[23]={0x00};
#elif defined leng_21
uint8_t leng=21;
uint8_t arr[21]={0x00};
#else
uint8_t leng=17;
uint8_t arr[17]={0x00};
#endif
void IR_Init(void)
{
P1DIR&=0XFE;//P1.0为输入模式
P1SEL|=0X01;//外设功能
}
void InitUart(void)
{
PERCFG &= 0xF0; //外设控制寄存器 USART 0的IO位置:0为P0口位置1
P0SEL = 0x0c; //P0_2,P0_3用作串口(外设功能)
P2DIR &= ~0XC0; //P0优先作为UART0
U0CSR |= 0x80; //设置为UART方式
U0GCR |= 11;
U0BAUD |= 216; //波特率设为115200
UTX0IF = 0; //UART0 TX中断标志初始置位0
}
void UartSendString(uint *Data, int len)
{
uint i;
for(i=0; i<len; i++)
{
U0DBUF = *Data++;
while(UTX0IF == 0);
UTX0IF = 0;
}
}
void InitT3(void)
{
T3CTL|=0X08;//开启溢出中断
T3IE=1;//开启总中断和T3中断
T3CTL|=0XE0;//128分频
T3CTL&=~0X03;//自动重装载
T3CTL|=0X10;//启动
EA=1;
}
void T1_Init(void)
{
PERCFG|=0X40;//定时器1备用位置2
P2SEL&=0XEF;//定时器1优先
T1CTL=0X0D;//128 自由运行模式
T1CCTL2=0X41;//上升沿捕获,捕获模式,定时器1通道2定时器使能
T1IE=1;
EA=1;
//定时器1溢出中断自动开启,TIMIF的寄存器当中
}
uint ary[3]={1,2,3};
int main()
{
CLKCONCMD &= ~0x40; //设置系统时钟源为32MHZ晶振
while(CLKCONSTA & 0x40); //等待晶振稳定为32M
CLKCONCMD &= ~0x07; //设置系统主时钟频率为32MHZ
IR_Init();
// Time1_Init();
T1_Init();
InitUart();
//UartSendString("usart is ok",11);
UartSendString(ary,3);
while(1)
{
if(receive_ok==0)
{
UartSendString(buffer, sizeof(buffer));
for(int ix=0;ix<200;ix++)
{
buffer[ix]=0x00;
}
receive_ok=1;
}
}
}
uint8_t a=0;
#pragma vector = T1_VECTOR
__interrupt void T1_ISR()
{
T1IF = 0;
T1STAT &= ~0x04;//清除中断标志位
// if(T1STAT&(~0XDF))//定时器 1溢出中断
// {
//
//
// irtime++;
//
// }
if(T1STAT&(~0XFB))//边沿触发中断,定时器1通道2中断
{
if(isUpCap)//判断是否是上升沿触发
{
a=T1CC2H;
uint8_t b=T1CC2L;
valueUp=(a<<8)|b;
isUpCap=0;//下降沿的标志位清除
T1CCTL2|=0X02;//下降沿捕获
irtime=0;//溢出计数值置0
}
else
{
uint8_t c=T1CC2H;
uint8_t d=T1CC2L;
valueDown=(c<<8)|d;
//valueDown=(T1CC2H<<8)|T1CC2L;
isUpCap=1;//上升沿的标志位清除
T1CCTL2|=0X01;//上升沿捕获
width=valueDown-valueUp+65536*irtime;//计算出时间
if(bufferId>=1)
{
buffer[bufferId++]=width;
if(bufferId>184)
{
bufferId=0;
receive_ok=0;
}
}
}
}
}
//#pragma vector = T3_VECTOR
//__interrupt void T3_ISR()//2.1ms
//{
// IRCON=0X00;
// irtime++;
//}