This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: CC2530 SBL 升级固件问题

Part Number: CC2530
Other Parts Discussed in Thread: Z-STACK

诸位大佬好,

先说需求:通过串口更新CC2530的固件,当前协议栈版本2.5.1a,计划是实现上位机对Z STACK 3.0.2与2.5.1a的自由切换

进度:参照文档“Serial Boot Loader for CC2530”,使用SerialBootTool成功实现了用串口写入固件的功能。且通过flash programmer二次确认数据写入没有问题。

问题点:原本能正常工作的程序,通过上述方案写入芯片之后,发现芯片无法正常工作(以ROUTER为例,发现其上电之后无法正常入网。)

我现在能确定程序是跳转成功的,已经从BOOT跳转至APP,但APP运行不正常。

我自认为是严格参照文档去修改的,有没有相似案例一起探讨下?是不是除了程序偏移,还有其他需要设置偏移量的?

此外,

想问下通过上述文档生成的hex,在没有拼接前段BOOT的情况下,直接用flash programmer烧入到芯片里,能正常工作吗?

  • 修正下问题描述:通过在线仿真发现程序卡在"HAL_BOARD_INIT"

    既trun off interrupts之后,就不运行了

  • 您好,

    感谢您的对TI产品的关注!为更加有效地解决您的问题,我需要多一些时间查看这个问题,稍后会为您解答。

  • 您好,

    根据描述,串行引导加载程序设计似乎按预期运行。您是否评估了没有引导加载程序的默认 Z-Stack 3.0.2 示例?您是尝试重新加入 Zigbee 3.0 网络还是尝试重新加入 2.5.1a 网络?

    由于安全不兼容,后者将无法实现。使用相同的 Zigbee 协议版本时,升级后重新加入是最有可能的。从我们的角度来看,HAL_Board_init 不会关闭中断,因此我们也不确定程序在哪里被卡住。您能否提供代码片段并指出您认为代码冻结的确切行?我建议在两个版本上都保留闪存串行引导加载程序,因为引导加载程序无法擦除自身并支持更多的串行固件更改选项。

    原文如下:Based on the description it appears that the Serial Boot Loader design is operating as intended.  Has the customer evaluated a default Z-Stack 3.0.2 example without the Boot Loader?  Are they attempting a fresh join to a Zigbee 3.0 network or trying to rejoin a 2.5.1a network?  The latter will not be possible because of security incompatibility.  Rejoins after upgrades are most possible when using the same Zigbee protocol version.  From my perspective, HAL_BOARD_INIT does not turn off interrupts so I am not certain where their program is stuck.  Can they provide code snippets and point to the exact line where they believe the code freezes?  I recommend retaining the flash Serial Boot Loader on both versions, as the Boot Loader cannot erase itself and to support further serial firmware change options.

  • 抱歉,前段时间个人原因项目停了一段时间,

    今天又试了下,疑似是新协议栈(Z-stack3.0.2)里面附带的Bootload工程不适配对Z stack2.5.1a的更新?

    我使用3.0.2的Bootlaod通过SBL升级了3.0.2下生成的GenericApp.bin,初步看来是正常的

    我又使用3.0.2的Bootlaod通过SBL升级了2.5.1a下生成的GenericApp.bin,能更新成功,且能跳转至应用程序,但应用程序无法正常运行

    3.0.2下的bootload是否如上述测试结果,不适用对2.5.1a进行SBL?

  • 是我本地应用配置的问题,,SBL与app需要配置成一样的,感谢关注!