This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shiqiu
CC2538芯片相关资料datasheet,user's guide在官网上都可以下载到,
现阶段CC2538支持的stack包括Z-Stack Home 1.1.0和TIMAC 1.5.0,后期会支持Z-Stark Smart Energy。
TIMAC提供了一个802.15.4兼容的MAC层协议栈,具体特性和适用环境可参考:http://www.ti.com/tool/timac
我能问一下,贵公司现在是准备采用CC2538做项目吗?还是在开发的过程中遇到了一些问题呢?
Hi Shiqiu,
推荐个ZigBee学习的网址给你:http://processors.wiki.ti.com/index.php?title=Low_Power_RF_Solutions
特别推荐其中的:
Hi Shiqiu
你说的是CC2538 Foundation Firmware是吧?!
因为CC2538是一个SoC,含有MCU在里面,基础固件提供了MCU外设等的驱动库函数以及SmartRF06EB平台的BSP。
对比于协议栈来说,基础固件提供了一个直接调用硬件层驱动radio模块去收发数据的例程
具体请参考:http://www.ti.com/tool/cc2538-sw下的description
Hi Shiqiu,
PER 是通过测试传输的丢包率来验证两个节点之间的链路状态的。
简单的来说就是两个节点一个发送,一个接收并回复ACK,它们约定好发送多少个包,比如1000个,然后统计收到了多少个ACK包以计算丢包率。
这个程序不复杂,可以直接看看了解具体测试流程。
CC2538的PER工程应该是根据SmartRF06EB平台做的,如果你手上的硬件不太相同,可能要做些对应的修改。