Other Parts Discussed in Thread: Z-STACK
/*********************************************************************
* @fn ZDP_IEEEAddrReq
*
* @brief This builds and send a IEEE_addr_req message. This
* function sends a unicast message looking for a 64
* bit IEEE address with a 16 bit address as bait.
*
* @param ReqType - ZDP_IEEEADDR_REQTYPE_SINGLE or
* ZDP_IEEEADDR_REQTYPE_EXTENDED
* @param SecurityEnable - Security Options
*
* @return afStatus_t
*/
afStatus_t ZDP_IEEEAddrReq( uint16 shortAddr, byte ReqType,
byte StartIndex, byte SecurityEnable )
{
uint8 *pBuf = ZDP_TmpBuf;
byte len = 2 + 1 + 1; // shortAddr + ReqType + StartIndex.
zAddrType_t dstAddr;
(void)SecurityEnable; // Intentionally unreferenced parameter
dstAddr.addrMode = (afAddrMode_t)Addr16Bit;
dstAddr.addr.shortAddr = shortAddr;
*pBuf++ = LO_UINT16( shortAddr );
*pBuf++ = HI_UINT16( shortAddr );
*pBuf++ = ReqType;
*pBuf++ = StartIndex;
return fillAndSend( &ZDP_TransID, &dstAddr, IEEE_addr_req, len );
}
在这个API函数中参数ReqType 的取值为 ZDP_IEEEADDR_REQTYPE_SINGLE 和 ZDP_IEEEADDR_REQTYPE_EXTENDED,但是在使用的时候编译不能通过,提示没有定义。望尽快解决。