This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的问题和他的问题类似的,只不过芯片型号不同。请问一下2630有没有类似2530的basicrf例子 - Zigbee 和 Thread 论坛 - Zigbee 和 Thread - E2E 设计支持 (ti.com)
您好,
现在官方提供的只有zstack的示例了,可以在2530与2538上使用。我们这边也无法给出更多了。
我们有查阅到:CC2530 and CC2538 host the same TI ZigBee stack, ie Z-Stack, running on top of OSAL.
The difference between the two devices address different application needs: CC2538 has more RAM, flash, integrates a CM3 and also has enhanced security engines. It is more suitable for high demanding applications which require more processing power as well as larger code-base.
However, from a pure ZigBee stack perspective, they are essentially the same.
我不确定商家的资料是什么时候的,也不确定是否可以通用在2538上。