這是我在TI網站上找到的code
PERCFG &= ~0x40; //select Timer 1 Alternative at Port 0 Location
PERCFG |= 0x03; //Move USART0 and USART1 to Alternative 2 Location
P2DIR = (P2DIR & ~0xC0) | 0X80; //Give priority to Timer 1
P0SEL |= 0x08; // SET P0_3 AS PERIPHERAL
T1CC0L = 0xFF; //PWM signal period
T1CC0H = 0x7F;
T1CC1L = 0x00; //PWM Duty Cycle, Channel 1 (P0_3)
T1CC1H = 0x01;
T1CCTL1 = 0x34; //Channel 1 in compare Mode, Set output on Compare down,
T1CTL |= 0x01; //Start the timer in free running Mode
但是我測出來的頻率都只有227Hz
請問要怎麼把頻率拉高呢?
大約在30k Hz附近就可以了
謝謝各位。