This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于如何最低功耗使用CC2530的问题

Other Parts Discussed in Thread: CC2530, Z-STACK

大家好,我在降低CC2530功耗的问题上有一点小麻烦。

应用的场景是这样的:红外热释电传感器+ Op-Amp(cc2530内置) + ADC. 每一秒读一次数据, 如果判断条件符合,再打开RF发送(一天也就发几十次),否则继续睡眠(PM3)。

这样的方法似乎还是不太能满足我的要求。感觉CPU每次醒来读数据的功耗高了一些。

我想问问能不能让CPU仅仅工作在32K RC下面,来实现超低功耗。或许这个问题比较小白,但还望大家解答一下。

如果有别的降低功耗方法,也请各位指教一下。

谢谢了!