我查过资料看着ti将会有一个zigbee ip协议栈,这个协议栈什么时候能够出来呢?对于现在的cc2538来说如果想实现网关功能需要怎么做呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The CC2538 device familiy currently supports TI’s ZigBee PRO stack Z-Stack™ with associated profiles and the ZigBee IP stack with
Smart Energy 2.0 profile.
CC2538的IP 协议栈是基于Smart Energy 2.0的。不过现在Z-Stack™ Energy还是1.1版本
我知道 “CC2538的IP 协议栈是基于Smart Energy 2.0的。不过现在Z-Stack™ Energy还是1.1版本” ,但是Smart Engergy2.0 什么时候能够出来呢?现在的Zstack能不能在别的系统上跑起来啊?
还有个问题就是如果cc2538用usb烧录程序需要怎么做?安装完SmartRF studio 7之后我这边不能够识别出cc2538,是不是我需要加一个ftdi芯片才能够用呢?
CC2538 是 M3的核,需要用JTAG to USB的仿真器 XDS100v3。
您好,再请教一个问题。
我用的CC2538 zstack-home 的uart串口问题。
按照下面初始化串口,串口并不能用:
halUARTCfg_t uartConfig;
uartConfig.baudRate = HAL_UART_BR_115200;
uartConfig.flowControl = FALSE;
uartConfig.callBackFunc = UART_CallBack;
HalUARTOpen (HAL_UART_PORT_0, &uartConfig);