Other Parts Discussed in Thread: TIMAC, Z-STACK, CC2530
请问下如何在TIMAC中配置协议栈进入PM3模式呢?感觉这方面的资料太少了,花了很长时间在研究这个,感觉收获不大,TI的工程师可以具体讲解下嘛?
多谢了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
参考下这个帖子 http://e2e.ti.com/support/low_power_rf/f/158/t/130489.aspx
可以具体点的分析下嘛?我现在是那样直接调用的,但是直接调用是无法进入PM2模式的。为什么HALSLEEP不能进入PM3模式而是PM2呢?请问下如果直接参数为0的话,也不行嘛?
请问下能给一份具体的配置低功耗的方案吗?我想通过P2.1和P2.2来分别设置进入和推出低功耗以及判断低功耗状态,但是我发现有问题,因为HALSLEEP里面有个IO中断,我想实现一秒拉低进入低功耗在拉低一秒推出不是那么灵敏,后来我通过两个IO来分配退出进入,虽然成功了,但是感觉不是我原先需要的效果。最让我头疼的是我用TIMAC1.3生成的hex文件和IAR直接下载的效果不一样(我采用的是cc2530 object banked),不知道为什么原因。生成hex文件,我是按照数据手册配置的