大家好,请教一下有关蜂鸣器的程序问题。
我在P1.3上装上蜂鸣器,需要以1K~3K之频率触发它,使其可发出声响,请问该如何进行呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,请教一下有关蜂鸣器的程序问题。
我在P1.3上装上蜂鸣器,需要以1K~3K之频率触发它,使其可发出声响,请问该如何进行呢?
感谢您的回复,
由于我现在是使用P1.2作为Buzzer,故若要使用定时器似乎是要使用Timer1,然而我目前发现CC2530与Buzzer相关之资料都是使用Timer3去驱动Buzzer,请问使用Timer1会有影响吗?
您好,
之后我先将Buzzer改至P1_6使用Timer3来做测试,将Code分为下列三部分
1. 初始化Buzzer之GPIO
void buzzerInit(void)
{
PERCFG |= 0x20; // Timer 3 Alternate location 2
P1DIR |= 0x40; // P1_6 = output
P1SEL |= 0x40; // Peripheral function on P1_6
T3CTL &= ~0x10; // Stop timer 3 (if it was running)
T3CTL |= 0x04; // Clear timer 3
T3CTL &= ~0x08; // Disable Timer 3 overflow interrupts
T3CTL |= 0x03; // Timer 3 mode = 3 - Up/Down
T3CCTL0 &= ~0x40; // Disable channel 0 interrupts
T3CCTL0 |= 0x04; // Ch0 mode = compare
T3CCTL0 |= 0x10; // Ch0 output compare mode = toggle on compare
}
2. 启动Buzzer
uint8 buzzerStart(uint16 frequency)
{
uint8 prescaler = 0;
// Get current Timer tick divisor setting
uint8 tickSpdDiv = (CLKCONSTA & 0x38)>>3;
// Check if frequency too low
if (frequency < (244 >> tickSpdDiv)){ // 244 Hz = 32MHz / 256 (8bit counter) / 4 (up/down counter and toggle on compare) / 128 (max timer prescaler)
buzzerStop(); // A lower tick speed will lower this number accordingly.
return 0;
}
// Calculate nr of ticks required to achieve target frequency
uint32 ticks = (8000000/frequency) >> tickSpdDiv; // 8000000 = 32M / 4;
// Fit this into an 8bit counter using the timer prescaler
while ((ticks & 0xFFFFFF00) != 0)
{
ticks >>= 1;
prescaler += 32;
}
// Update registers
T3CTL &= ~0xE0;
T3CTL |= prescaler;
T3CC0 = (uint8)ticks;
// Start timer
T3CTL |= 0x10;
return 1;
}
3. 停止Buzzer
void buzzerStop(void)
{
T3CTL &= ~0x10; // Stop timer 3
}
但当我按下触发键启动buzzerStart,还是无法使用蜂鸣器,请问我是有何处忽略了吗?
P.S. 我frequency给2000
参考下这个帖子 http://e2e.ti.com/support/low_power_rf/f/155/t/92359.aspx
再次感謝您的回覆
後來我參考了http://e2e.ti.com/support/low_power_rf/f/158/t/291670.aspx?pi267162=1
Buzzer已可發聲