Other Parts Discussed in Thread: Z-STACK
大家好~
我想在zstack 2530 2.3.0-1.4.0的end device 用Time3 控制P1.3输出一个PWM波形。在裸机上已经实现功能,但是在协议栈里加入同样的代码后就不行了,困惑了好几天~ 希望大家能帮下~ 谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: Z-STACK
大家好~
我想在zstack 2530 2.3.0-1.4.0的end device 用Time3 控制P1.3输出一个PWM波形。在裸机上已经实现功能,但是在协议栈里加入同样的代码后就不行了,困惑了好几天~ 希望大家能帮下~ 谢谢~
方便把代码贴出来吗?这里贴一份使用timer 3控制p1.4的代码:
PERCFG &= (~(0x20)); // Select Timer 3 Alternative 1 location
P2SEL |=0x20;
P2DIR |= 0xC0; // Give priority to Timer 1 channel2-3
P1SEL |= BV(4); // Set P1_0 to peripheral, Timer 1,channel 2
P1DIR |= BV(4);
T3CTL &= ~0x10; // Stop timer 3 (if it was running)
T3CTL |= 0x04; // Clear timer 3
T3CTL &= ~0x08; // Disable Timer 3 overflow interrupts
T3CTL |= 0x03; // Timer 3 mode = 3 - Up/Down
T3CCTL1 &= ~0x40; // Disable channel 0 interrupts
T3CCTL1 |= 0x04; // Ch0 mode = compare
T3CCTL1 |= 0x10; // Ch0 output compare mode = toggle on compare
T3CTL &= ~0xE0; // Clear Prescaler divider value
T3CTL |= 0xA0; //Set Prescaler divider value = Tick frequency /32
T3CC0 = 128; //Set ticks = 128
// Start timer
T3CTL |= 0x10;
谢谢回复,已经可以了~不过最终还是参照ZLL里Timer1 的控制,再加自己修改,才实现的。下面的ZLL里的timer1初始化代码
T1CCTL0 = 0; /* Make sure interrupts are disabled */
T1CCTL1 = 0; /* Make sure interrupts are disabled */
T1CCTL2 = 0; /* Make sure interrupts are disabled */
T1CCTL3 = 0; /* Make sure interrupts are disabled */
T1CCTL4 = 0; /* Make sure interrupts are disabled */
/* Setup prescale & clock for timer0 */
halTimerRecord[HW_TIMER_1].prescale = HAL_TIMER1_16_PRESCALE;
halTimerRecord[HW_TIMER_1].clock = HAL_TIMER_32MHZ;
halTimerRecord[HW_TIMER_1].prescaleVal = HAL_TIMER1_16_PRESCALE_VAL;
/* Setup Timer1 Channel structure */
halTimer1Channel[0].TxCCTL = TCHN_T1CCTL;
halTimer1Channel[0].TxCCL = TCHN_T1CCL;
halTimer1Channel[0].TxCCH = TCHN_T1CCH;
halTimerRecord[HW_TIMER_1].configured = TRUE;
halTimerRecord[HW_TIMER_1].opMode = HAL_TIMER1_OPMODE_UPDOWN;
halTimerRecord[HW_TIMER_1].channel = 0;
halTimerRecord[HW_TIMER_1].channelMode = 0;
halTimerRecord[HW_TIMER_1].intEnable = FALSE;
halTimerRecord[HW_TIMER_1].callBackFunc = cBack;
Timer1MaxCount = halTimer1SetPeriod (4292); // 233Hz
halTimerSetPrescale (HW_TIMER_1, halTimerRecord[HW_TIMER_1].prescale);
halTimerSetChannelMode (HW_TIMER_1, halTimerRecord[HW_TIMER_1].channelMode);
halTimer1SetChannelCCTL(HAL_T1_CH0, 0, 1, HAL_TIMER1_CH0_CMP_MODE_SET_ON_COMP, 1, HAL_TIMER1_CH_CAP_MODE_NO);
halTimer1SetChannelCCTL(HAL_T1_CH1, 0, 1, HAL_TIMER1_CHn_CMP_MODE_CLR_ON_COMP_SET_ON_0, 1, HAL_TIMER1_CH_CAP_MODE_NO);
halTimer1SetChannelCCTL(HAL_T1_CH2, 0, 1, HAL_TIMER1_CHn_CMP_MODE_CLR_ON_COMP_SET_ON_0, 1, HAL_TIMER1_CH_CAP_MODE_NO);
halTimer1SetChannelCCTL(HAL_T1_CH3, 0, 1, HAL_TIMER1_CHn_CMP_MODE_CLR_ON_COMP_SET_ON_0, 1, HAL_TIMER1_CH_CAP_MODE_NO);
halTimer1SetChannelCCTL(HAL_T1_CH4, 0, 1, HAL_TIMER1_CHn_CMP_MODE_CLR_ON_COMP_SET_ON_0, 1, HAL_TIMER1_CH_CAP_MODE_NO);
halTimer1SetChannelDuty (HAL_T1_CH1, 0);
halTimer1SetChannelDuty (HAL_T1_CH2, 0);
halTimer1SetChannelDuty (HAL_T1_CH3, 0);
halTimer1SetChannelDuty (HAL_T1_CH4, 0);
/* set timer 1 operating mode */
T1CTL &= ~(HAL_TIMER1_OPMODE_BITS);
T1CTL |= HAL_TIMER1_OPMODE_UPDOWN;
你好,我正在学习zigbee,准备在z-stack中添加Timer1定时中断,采样ADC数据,但是参考hal_timer.c中的函数,还是没有实现进入timer1的回调函数。请问这个ZLL中是如何实现timer1操作的?能否将代码给我发一份:675412313@qq.com,谢谢啦!
To michael XU
如果你用了协议栈,那么建议用osal的定时函数来完成这个工作,不需要在硬件层操作定时器 osal_start_timerEx( )