Other Parts Discussed in Thread: CC2538
i'm study the "gateway" solution , now the demo could works .
but in order to learn more about this solution , we want to open the MT function .
my steps as bellow : [ zstack 1.1.0, z-tools2.0, usb to serial cable]
1> add preprocessor symbles in the"gateway" project options.
ewarm
SECURE=1
HAL_UART=TRUE
ZTOOL_P1
MT_TASK
MT_SYS_FUNC
MT_ZDO_FUNC
MT_UART
MT_UTIL_FUNC
MT_AF_FUNC
MT_NWK_FUNC
LCD_SUPPORTED=DEBUG
CC2538_USE_ALTERNATE_INTERRUPT_MAP=1
HAL_LCD=FALSE
SELECT_TEST
2> disable the flowcontrol in the file MT_UART.c
#if 0
#ifdef ZNP_UART_TEST
uartConfig.flowControl = FALSE;
#else
uartConfig.flowControl = TRUE;
#endif
#else
uartConfig.flowControl = FALSE;
#endif
3> compile and download the binary into CC2538
4> open the Ztool2.0 with " datebits:8 rate:38400 parity:none handshake:none stopbits:1 " , but it can't find the devices at all.
so could anyone help to check if there were something wrong ? and what's the right settings for "gateway" to enable|open MT function
thank you .