This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

2530的LQI 和RSSI 分别在什么范围是认为可以连接网络和发送的呢?

请问各位老师,2530的LQI 和RSSI 分别在什么范围是认为可以连接网络和发送的呢

  • IEEE 802.15.4 标准要求的LQI值限制在范围0到255,至少需要8个唯一的值。当设置MDMCTRL0.AUTOCRC,前8个符号的平均相关值连同RSSI和CRC OK/not OK,附加到每个收到的帧中。相关值110表示最高质量帧,而值50一般表示无线电检测到的最低质量帧。