This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

基于simpliciTI的点对点对等网络实验 simple_peet_to_peer



今天拿来TI的例程simple_Peer_to_Peer.做点对点对等网络实验,将LinkTo.c和LinkListen.c程序分别下载给两个ED后。
talker上电后,红绿LED同时点亮,按下按键s1\s2中任意一个,红绿LED同时闪烁,进入发送link广播帧
状态;
listener上电后,红绿LED同时点亮,按下按键s1\s2中任意一个,绿色LED熄灭,红色LED仍然点亮,进入侦听link信息状态;
但很遗憾的时,当两个ED靠近时,连接始终建立不起来,无法进行通信。

talker一直停在while (SMPL_SUCCESS != SMPL_Link(&sLinkID1))这里,也就是说,该ED一直在发送link广播帧等待应答;

而listener则一直停在if (SMPL_SUCCESS == SMPL_LinkListen(&sLinkID2)),这里,也就是说,该ED一直在侦听来自talker的link信息。

但不论两个ED距离远近,始终建立不起连接。

一开始我以为是因为两个ED的物理地址可能设置成一样了,但是我后来又重新给它们分别下载程序,确定talker的地址为{0x79, 0x56, 0x34, 0x12};

listener的地址为{0x79, 0x56, 0x34, 0x13},确实给它们设置了不同的物理地址。

但还是建立不起连接,不知为何?

所采用的源程序是simpliciTI-IAR-1.2.0的simple_Peer_to_Peer

希望前辈能指点一下!!先谢过