This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ZIGBEE 开发遇到的问题



1、都遵守了HA规范,但明显有厂家设备不兼容及不能入网的问题怎么解决。

2、PANID 在设置了NV后仍然发生变化,且周期不固定。

3、在使用2.3及2.5协议栈时发现,组播对节点设备没有效果,这是什么原因。路由器可以收到。

4、怎样方便的找到整个ZIGBEE网络中的节点。(遍历或广播?)

  • 你好,

    1)如果都遵守ZHA规范,并且产品已经通过ZigBee联盟认证测试,那肯定是可以互通互联的。如果说是遵守ZHA规范,但是没有去过测试认证,所以具体里面做了什么就不知道了。

    2)请问你是怎么设置的?直接协调器端开启NV功能,第一次上电建立一个网络?第二次再上电建立一个网络发现PANID变了???如果是这样的话,原因在于第一次建立的网络没有任何设备加入过,有设备加过以后就不会改PANID了。

    3)Groupcast message 是indirect message, 如果是Rx Always on的设备可以直接收到,因为Rx一直处于打开状态,End Device的Rx 不是Always on的,有可能处于休眠状态,所以需要等End Device向父节点data request的时候,才会把数据发出去

    4)通过子节点找子节点 请找C:\Texas Instruments\Z-Stack Home 1.2.0\Documents\Method for Discovering Network Topology.pdf