This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:cc2530, uart 接收串口数据异常

Other Parts Discussed in Thread: CC2530

genericapp;  2.5.1a

CC2530,回复收到的信息给PC

现象: pc串口助手发送不同长度的内容给CC2530,但每次只收到一个0X00;  

//1

void MyUart0Init(void)
{
halUARTCfg_t uartConfig;

uartConfig.configured = TRUE;
uartConfig.baudRate = HAL_UART_BR_57600;
uartConfig.flowControl = FALSE;
uartConfig.flowControlThreshold = 80;
uartConfig.rx.maxBufSize = 128;
uartConfig.tx.maxBufSize = 128;

uartConfig.idleTimeout = 6;
uartConfig.intEnable = TRUE;
uartConfig.callBackFunc = RxUart0Data_CB;

HalUARTOpen (HAL_UART_PORT_0, &uartConfig);
}

//2

static void RxUart0Data_CB( uint8 port, uint8 event ) //UART0串口回调函数
{
uint8 buf = 0;

while ( Hal_UART_RxBufLen(HAL_UART_PORT_0))
{
HalUARTRead(HAL_UART_PORT_0,&buf,1);
HalUARTWrite(HAL_UART_PORT_0,&buf,1);

}

}

//3

GenericApp_Init

{

...

MyUart0Init();

HalUARTWrite(0,"BOOT...\n",8);   //此处能正常输出到串口助手。

}