Other Parts Discussed in Thread: CC2530, TIMAC
协议栈:ZSTACK 2.5.0
睡眠设备 POLL_RATE:1000ms
测试时发现:10个睡眠设备在接收协调器(父节点)的广播包时,有一个设备没能接收到。协调器清除NV后重新发送广播包,所有设备都能接收到。
问题:1.为什么会出现测试的情况?
2.CC2530协调器在POLL_RATE 为1S情况,大概能挂在多少个?
3.协调器(父节点)缓存给子节点的信息在那个参数能找到?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1,由于节点开启了休眠功能,那么节点发送Data request以后Rx打开的时间比不休眠的时候肯定要短,所以你的10个节点同时data request请求数据的时候,由于碰撞重发,有可能那时候节点已经进入休眠了。
2,如果是你这种的星型网络的话,100个肯定没有问题的,如果你只使用星型网络,建议使用TIMAC协议栈
3,
/* Default indirect message holding timeout value:
* 1-65535 (0 -> 65536) X CNT_RTG_TIMER X RTG_TIMER_INTERVAL
*/
-DNWK_INDIRECT_MSG_TIMEOUT=7