This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于cc2530中断唤醒休眠的问题,请各位帮忙解决下!

我在协议栈中修改了串口0 你能中断唤醒休眠,并且能从串口0 读出正确的数据,但是串口1就不行,我串口0的修改如下:在休眠前加入

P0SEL &= ~0X20; //外P0_5为通用接口模式

 GPIO P0DIR &= ~0X20; //P0_5为输入

P0IEN |= 0X20; //开P0_5的IO中断使能

 IEN1 |= 0X20; //开P0的中断

休眠后理解恢复到串口的原始状态,

P0SEL = 0x3C; 

 GPIO P0DIR =0X01;

P0IEN = 0X00;

 IEN1 = 0X04;

hal_board_cfg.h头文件中,修改如下:

注掉原有的

#define HAL_UART_ISR  1//重新定义为ISR模式

这样就能从休眠中唤醒,

我串口1修改如下:在不休眠的时候,通过修改

hal_board_cfg.h头文件中,

#define HAL_UART_ISR  2//重新定义为ISR模式

这样就能正常读出数据,

加入休眠,我修改如下:

在休眠前加入

 P1SEL &= ~0X80; //外P1_7为通用接口模式 GPIO   P1DIR &= ~0X80; //P1_7为输入

  P1IEN |= 0X80; //开P1_7的IO中断使能   IEN2 |= 0X80; //开P1的中断

休眠后醒来后立即回复原始状态:

P1SEL ^= 0x80;

GPIO   P1DIR ^= 0X17;

  P1IEN &= ~ 0X00; 

   IEN2 &= ~0X09;

但是这样不能从休眠中唤醒,更不要提读出数据了,请各位大神帮我看看是不是串口1的配置 出现了问题,谢谢