This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Z-stack AF_DataRequest 最大字节发送问题

Other Parts Discussed in Thread: Z-STACK

在Z-stack中,我们调用数据发送函数,可以发送的最大字节数即ASDU最大是多少呢?

在f8wConfig.cfg文件中定义了
/* Set the MAC MAX Frame Size (802.15.4 default is 102) */


-DMAC_MAX_FRAME_SIZE=116
我做测试却是最大可以发送99字节,并且修改了MAC_MAX_FRAME_SIZE值后并没有影响,所以搞不懂了。

通过AF_DataRequest发送的数据长度超过MAC_MAX_FRAME_SIZE,将会出现很大的延时,或直接发送不成功


怎么才能增加 

Z-stack AF_DataRequest()发送字节的长度