Other Parts Discussed in Thread: CC2530, Z-STACK
我没有用dongle的usb和bb连接。而是自己做了一个usb转串口,把cc2530和bb连在一起。
u转串在bbb上识别为ttyUSB0,而server用的是ttyACM0.
请问怎么让server用ttyUSB0 ?
Below are the logs when starting servers:
oot@am335x-evm:~/z-stack_linux_gateway_arm_binaries/servers# ./zigbeeHAgw bbb
running zigbeegw.scr on an ARM resetting beaglebone black sleeping 6 seconds after reset...
[ 65.277339] usb 2-1: USB disconnect, device number 2
[ 65.285478] ftdi_sio ttyUSB0: FTDI USB Serial Device converter now disconnected from ttyUSB0
[ 65.295731] ftdi_sio 2-1:1.0: device disconnected
[ 65.577660] usb 2-1: new full-speed USB device number 3 using musb-hdrc
[ 65.724744] usb 2-1: New USB device found, idVendor=0403, idProduct=6001
[ 65.731802] usb 2-1: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ 65.739298] usb 2-1: Product: USB Serial Converter [ 65.744326] usb 2-1: Manufacturer: FTDI
[ 65.748359] usb 2-1: SerialNumber: FTFY7QC2
[ 65.759780] ftdi_sio 2-1:1.0: FTDI USB Serial Device converter detected
[ 65.766861] usb 2-1: Detected FT232RL
[ 65.770761] usb 2-1: Number of endpoints 2
[ 65.775063] usb 2-1: Endpoint 1 MaxPacketSize 64
[ 65.779915] usb 2-1: Endpoint 2 MaxPacketSize 64
[ 65.784758] usb 2-1: Setting MaxPacketSize 64
[ 65.797965] usb 2-1: FTDI USB Serial Device converter now attached to ttyUSB0
Using serial port: /dev/ttyACM0 /dev/ttyACM0: No such file or directory /dev/ttyACM0
open failed /dev/ttyACM0: No such file or directory /dev/ttyACM0
open failed done stty: can't open '/dev/ttyACM0': No such file or directory
stty: can't open '/dev/ttyACM0': No such file or directory
Starting the ZigBee gateway subsystem deviceKey = 0 (0 ) devPath = '/dev/ttyACM0' logPath = './NpiLnxLog.txt' ... f
reeing memory (ret 0) Port: 2533 Following IP addresses are available:
IPv4: interface: lo IP Address 127.0.0.1 The socket will listen on the following IP addresses:
IPv4: 0.0.0.0 IPv6: :: 0.0.0.0 means it will listen to all available IP address
waiting for first connection on #3... NPI started (pid 1437) at Mon Mar 31 17:28:29 UTC 2014
Connected to #5.(127.0.0.1 / ::381c:f3b6:f01d:f3b6) ZLSZNP started (pid 1444) at Mon Mar 31 17:28:33 UTC 2014
[NWK_MGR/MAIN] : there are 2 args
[NWK_MGR/MAIN] : argv[0] = ./NWKMGR_SRVR_arm
[NWK_MGR/MAIN] : argv[1] = 127.0.0.1:2536
[NWK_MGR/MAIN] : ************************************************ [NWK_MGR/MAIN] : * Network Manager Server v1.0.1 *
[NWK_MGR/MAIN] : * The following are the avaible key commands: * [NWK_MGR/MAIN] : * Exit Program. - q *
[NWK_MGR/MAIN] : ************************************************
NETWORK MANAGER started (pid 1452) at Mon Mar 31 17:28:34 UTC 2014
[GATEWAY/MAIN] :
[GATEWAY/MAIN] : ************************************************
[GATEWAY/MAIN] : * Gateway Server v1.0.1 *
[GATEWAY/MAIN] : * The following are the avaible key commands: * [GATEWAY/MAIN] : * Exit Program. - q *
[GATEWAY/MAIN] : ************************************************
GATEWAY SERVER started (pid 1460) at Mon Mar 31 17:28:36 UTC 2014
[OTASRVR/MAIN] : [OTASRVR/MAIN] : ************************************************ [OTASRVR/MAIN] : * OTA Upgrade Server 1.0.1 * [OTASRVR/MAIN] : * The following are the avaible key commands: * [OTASRVR/MAIN] : * Exit Program. - q *
[OTASRVR/MAIN] : ************************************************
[NWK_MGR/MAIN] ERROR: Endpoint Registration Failed
[NWK_MGR/MAIN] ERROR: Reading Local Network Information Failed
[NWK_MGR/MAIN] : Initialization failed. Quitting now. mhoyt
OTA SERVER started (pid 1470) at Mon Mar 31 17:28:38 UTC 2014
[OTASRVR/MAIN] : Error - Could not register OTA endpoint with zstackserver.Exiting...
starting tracker with our pid ./zigbeeHAgw and pid list 1437 1444 1460 1470 ===================================================
NETWORK MANAGER exited with code 255 at Mon Mar 31 17:28:38 UTC 2014