Other Parts Discussed in Thread: CC2591, CC2530
大家好,现在做东西想发挥zigbee低功耗的功能,终端节点,采用CC2530,加入了CC2591功放,协议栈版本为TI ZStack-CC2530-2.3.0-1.4.0,在hal_board_cfg.h中修改xHAL_PA_LNA为HAL_PA_LNA开启功放,在f8wConfig.cfg中修改-DRFD_RCVC_ALWAYS_ON=FALSE,在官方协议栈Sample中修改OSAL_PwrMgr.c文件中的void osal_pwrmgr_init( void )函数pwrmgr_attribute.pwrmgr_device = PWRMGR_BATTERY; 开启低功耗。在运行时,我通过串口将休眠模式打印出来,发现大概每隔不到一秒左右串口打印的信息为02,03,03,03,03,这表示有时工作在PM2模式有时工作在PM3模式下。Sample工程我设置了两个按键,均是外部中断方式,只有在按键按下时才会发送点对点信息到协调器,请问是哪个进程运行使系统工作在PM2模式的?还有就是如果工作在这样的情况下,一节3.7v的650mh的锂电池在极少按按键的情况下能够使其工作多长时间。