This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530与WIFI芯片同在一个PCB上,应该怎么解决干扰问题?

Other Parts Discussed in Thread: CC2530

我们把CC2530协调器集成在WIFI无线路由器上,现在遇到了干扰问题,通过抓包可以看到,节点向协调器发送了数据,但是协调器没有回复ACK。但是当WIFI负荷不大的时候,节点可以成功把数据发到协调器,而且协调器的RSSI指示也是在-55dbm ~ -60dbm这个范围。

1,Zigbee不是有CSMA么?为什么节点的CSMA没有检测到WIFI的冲突?

2,协调器的天线和WIFI天线,之间应该保持多远的距离?

  • Aries,

    1,要看WiFi工作的信道是否是对ZIgBee影响较大的几个信道?

    2,至少是不同的朝向,具体多少距离没有测试过。

    另外如果可以的话,建议在软件上做共存机制,也就是每次保证ZigBee的数据优先,因为WiFi基于tcp通信的话,失败可以重传。