This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Z-Stack Lighting 1.0.2 中PWM 的亮度为何 限定不能100%?

void halTimer1SetChannelDuty (uint8 channel, uint16 promill)
{
#define MIN_PROMILL 20
uint16 count;

if (promill < MIN_PROMILL)
promill = 0;

/* Load count = ((sec/tick) x clock) / prescale */
count = (uint16)( ((uint32)(Timer1MaxCount) * promill + 500)/ 1000 );
count = ( (count >= Timer1MaxCount) ? Timer1MaxCount-1 : (count == 0 ? 1 : count) );

halTimer1SetChannelCount(channel, count);
}

count 限定 Timer1MaxCount - 1 到 1之间。

请教下!