This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ZStack-CC2530-2.3.0-1.4.0 系统时钟初始化



osal中timer初始化:

void osalTimerInit( void )
{
  osal_systemClock = 0;
}

hal中初始化:

typedef struct
{
  bool configured;
  bool intEnable;
  uint8 opMode;
  uint8 channel;
  uint8 channelMode;
  uint8 prescale;
  uint8 prescaleVal;
  uint8 clock;
  halTimerCBack_t callBackFunc;
} halTimerSettings_t;

typedef struct
{
  uint8 volatile XDATA *TxCCTL;
  uint8 volatile XDATA *TxCCH;
  uint8 volatile XDATA *TxCCL;
  uint8 volatile XDATA *TxOVF;
  uint8 ovfbit;
  uint8 intbit;
} halTimerChannel_t;

/*********************************************************************
 * GLOBAL VARIABLES
 */
static halTimerSettings_t halTimerRecord[HW_TIMER_MAX];
static halTimerChannel_t  halTimerChannel[HW_TIMER_MAX];

void HalTimerInit (void)
{
  T1CCTL0 = 0;    /* Make sure interrupts are disabled */
  T1CCTL1 = 0;    /* Make sure interrupts are disabled */
  T1CCTL2 = 0;    /* Make sure interrupts are disabled */
  T3CCTL0 = 0;    /* Make sure interrupts are disabled */
  T3CCTL1 = 0;    /* Make sure interrupts are disabled */
  T4CCTL0 = 0;    /* Make sure interrupts are disabled */
  T4CCTL1 = 0;    /* Make sure interrupts are disabled */

  /* Setup prescale & clock for timer0 */
  halTimerRecord[HW_TIMER_1].prescale    = HAL_TIMER1_16_PRESCALE;
  halTimerRecord[HW_TIMER_1].clock       = HAL_TIMER_32MHZ;
  halTimerRecord[HW_TIMER_1].prescaleVal = HAL_TIMER1_16_PRESCALE_VAL;

  /* Setup prescale & clock for timer2 */
  halTimerRecord[HW_TIMER_3].prescale    = HAL_TIMER3_8_PRESCALE;
  halTimerRecord[HW_TIMER_3].clock       = HAL_TIMER_32MHZ;
  halTimerRecord[HW_TIMER_3].prescaleVal = HAL_TIMER3_8_PRESCALE_VAL;

  /* Setup prescale & clock for timer3 */
  halTimerRecord[HW_TIMER_4].prescale    = HAL_TIMER4_8_PRESCALE;
  halTimerRecord[HW_TIMER_4].clock       = HAL_TIMER_32MHZ;
  halTimerRecord[HW_TIMER_4].prescaleVal = HAL_TIMER4_8_PRESCALE_VAL;

  /* Setup Timer1 Channel structure */
  halTimerChannel[HW_TIMER_1].TxCCTL =  TCHN_T1CCTL;
  halTimerChannel[HW_TIMER_1].TxCCL =   TCHN_T1CCL;
  halTimerChannel[HW_TIMER_1].TxCCH =   TCHN_T1CCH;
  halTimerChannel[HW_TIMER_1].TxOVF =   TCNH_T1OVF;
  halTimerChannel[HW_TIMER_1].ovfbit =  TCHN_T1OVFBIT;
  halTimerChannel[HW_TIMER_1].intbit =  TCHN_T1INTBIT;

  /* Setup Timer3 Channel structure */
  halTimerChannel[HW_TIMER_3].TxCCTL =  TCHN_T3CCTL;
  halTimerChannel[HW_TIMER_3].TxCCL =   TCHN_T3CCL;
  halTimerChannel[HW_TIMER_3].TxCCH =   TCHN_T3CCH;
  halTimerChannel[HW_TIMER_3].TxOVF =   TCNH_T3OVF;
  halTimerChannel[HW_TIMER_3].ovfbit =  TCHN_T3OVFBIT;
  halTimerChannel[HW_TIMER_3].intbit =  TCHN_T3INTBIT;

  /* Setup Timer4 Channel structure */
  halTimerChannel[HW_TIMER_4].TxCCTL =  TCHN_T4CCTL;
  halTimerChannel[HW_TIMER_4].TxCCL =   TCHN_T4CCL;
  halTimerChannel[HW_TIMER_4].TxCCH =   TCHN_T4CCH;
  halTimerChannel[HW_TIMER_4].TxOVF =   TCNH_T4OVF;
  halTimerChannel[HW_TIMER_4].ovfbit =  TCHN_T4OVFBIT;
  halTimerChannel[HW_TIMER_4].intbit =  TCHN_T4INTBIT;
}
void InitBoard( uint8 level )
{
  if ( level == OB_COLD )
  {
    // Interrupts off
    osal_int_disable( INTS_ALL );
    // Turn all LEDs off
    HalLedSet( HAL_LED_ALL, HAL_LED_MODE_OFF );
    // Check for Brown-Out reset
    ChkReset();
  }
  else  // !OB_COLD
  {
    /* Initialize Key stuff */
    OnboardKeyIntEnable = HAL_KEY_INTERRUPT_DISABLE;        //DISABLE
    HalKeyConfig( OnboardKeyIntEnable, OnBoard_KeyCallback);
  }
}

这里也没有

我把hal_timer.h中HalTimerConfig和HalTimerStart屏蔽了也没有报错

请问系统时钟是在哪里开启的

  • 这个是定时器的使用初始化。

    SLEEPCMD &= ~OSC_PD; /* turn on 16MHz RC and 32MHz XOSC */ \
    while (!(SLEEPSTA & XOSC_STB)); /* wait for 32MHz XOSC stable */ \
    asm("NOP"); /* chip bug workaround */ \
    for (i=0; i<504; i++) asm("NOP"); /* Require 63us delay for all revs */ \
    CLKCONCMD = CLKCONCMD_VALUE; /* Select 32MHz XOSC and the source for 32K clock */ \
    while (CLKCONSTA != CLKCONCMD_VALUE); /* Wait for the change to be effective */ \
    SLEEPCMD |= OSC_PD; /* turn off 16MHz RC */

    系统时钟是根据MAC Timer来更新的。

    void osal_run_system( void )
    {
    uint8 idx = 0;

    osalTimeUpdate();
    ...

    }