This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DONGLE程序每4秒向串口发出指令:FE 09 09 00 14 8A 01 4F 04 01 00 0E 0B D0
即PAN:0x044F。 Addr:0x0001。
请教下,OtaServer这个工具的判定规则是怎么样的。
附图:
3.修改流控,因为国产开发板硬件不支持流控
修改MT_UART.c文件的MT_UartInit()函数
uartConfig.configured = TRUE;
uartConfig.baudRate = MT_UART_DEFAULT_BAUDRATE;
uartConfig.flowControl = MT_UART_DEFAULT_OVERFLOW; 修改宏定义,改为FALSE
uartConfig.flowControlThreshold = MT_UART_DEFAULT_THRESHOLD;
uartConfig.rx.maxBufSize = MT_UART_DEFAULT_MAX_RX_BUFF;
uartConfig.tx.maxBufSize = MT_UART_DEFAULT_MAX_TX_BUFF;
uartConfig.idleTimeout = MT_UART_DEFAULT_IDLE_TIMEOUT;