如:我使用的CC2530的GPIO寄存器的P1端口的第一个引脚P1_1,现在我使用的是CC2538控制器,我想使用PD端口的第一个引脚PD1,我该如何编写?
CC2530:P1_1 = 0x1;
CC2538:不知道怎么写
谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以下载 CC2538的例程 http://www.ti.com.cn/tool/cn/cc2538-sw
Susan Yang你好
CC2530的PI_1是不是相同于HWREG(GPIO_D_BASE+ (GPIO_O_DATA + (GPIO_PIN_1<< 2)))
如果我想进行判断if(P1_1){}时,好像if(HWREG(GPIO_D_BASE+ (GPIO_O_DATA + (GPIO_PIN_1<< 2)))){}进不去
还有函数IOCPadConfigSet(ui32Port, ui8Pins, IOC_OVERRIDE_DIS);有什么作用,看不明白,Pad又是什么
你好!
我遇到了如下问题:
1.用CC2530做协调器,CC2538做终端进行无线通信,2530用的协议栈是ZStack-CC2530-2.3.0-1.4.0,2538用的协议栈是Z-Stack Mesh 1.0.0,程序很简单,就是在终端入网后(网络状态变成DEV_END_DEVICE)启动一个周期性循环的消息,通过无线发一串数据给协调器,但没有实现,请问是不是不同的协议栈进行通信需要特殊注意的地方?
2.在一个帖子里看到您提到2538和2530通信建议使用相同的协议栈,他们一个是51,一个是arm,好像没有这样的协议栈吧?
3.2538 的协议栈里面的串口配置有没有TI官方的例程?
shaoxin cui1你好:
1、我记得我上一个工作的一个项目就用过,使用zstack-2007的协议栈,因为这个协议栈是支持30和38的,在30上不用做修改,但在38上就必须将硬件部分做出修改才可以组网和通讯。
2、你可以去官网查找一下同时支持2530和2538的协议栈,我第一条已经描述了。
3、2538官方有提供串口配置例程