请问大神们,这个问题怎么解决呢:Error[e16]: Segment RAM_CODE_FLASH (size: 0x27 align: 0) is too long for segment definition. At least 0x4 more bytes needed. The problem occurred while processing the
segment placement command "-Z(CODE)RAM_CODE_FLASH=_RAM_CODE_FLASH_START-_RAM_CODE_FLASH_END", where at the moment of placement the
available memory ranges were "CODE:39edd-39eff"
Reserved ranges relevant to this placement:
CODE:39edd-39eff RAM_CODE_FLASH
BIT:0-7 BREG
BIT:80-97 SFR_AN
BIT:a0-af SFR_AN
BIT:b8-c7 SFR_AN
BIT:d8-df SFR_AN
BIT:e8-ef SFR_AN
Error while running Linker