This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
CC2538使用Z-Stack Home 1.2.0协议栈JLink调试时出现_hal_uart_isr.c中的uint8 HalUARTOpenIsr(uint8 port, halUARTCfg_t *config)函数中的UARTConfigSetExpClk(HAL_UART_PORT, SysCtrlClockGet(), UBRRTable[uartRecord.baudRate],(UART_CONFIG_WLEN_8 | UART_CONFIG_PAR_NONE | UART_CONFIG_STOP_ONE));这句通不过,MT_UartInit();这个函数注掉,osal_init_system();才可以正常运行,请问各位大神,这需要怎么修改?
现在我使用官方提供的XDS调试器,使用Z-Stack Home 1.2.0协议栈,可是串口一直不能用,宏定义使用的是ZTOOL_P1,使用HalUARTWrite(ZTOOL_PORT,"bbbb",4);串口打印不出来东西,请问各位大神是怎么回事?
我打印的地方是static void zclSampleLight_HandleKeys( byte shift, byte keys );这个函数里面的按键控制的,不可能没有初始化的,我不知道应该怎么设置UART呢?