This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

真诚求教我们这种应用用蓝牙4.0BLE还是Zigbee?

大家好,我们是做智能家居的创业小团队,之前没有多少无线相关经验。
我们做的智能设备用4节5号电池供电,希望至少一年换一次电池。设备需要全天候和网络保持连接,以便及时上传数据到后台,设备也要能响应用户在远程通过万络传来的操作信息。数据传输频率不高,一天<10次,数据量也很小。我们的初步计划是,CPU空闲时处于standby模式(实测耗电几个uA),在网络要和设备交换数据时,由无线模块将CPU唤醒。无线模块也需要尽量省电(空闲时也能<10uA),最好能平时也处于深度休眠状态,隔几秒钟去自动扫描网络,看是否有针对设备的数据请求。
CPU通过市场上现成的串口无线模块与家里的专用无线网关(基站)相连,网关与互联网连接。
现在不知道是用蓝牙4.0BLE还是Zigbee作为无线方案。
我们目前总结的蓝牙4.0BLE的优点是:
1)现在是越来越流行的趋势
2)能直接与手机相连。
缺点是:
1)市面上没找到现成的蓝牙4.0转以太网的基站。有人能给推荐吗?
2)打听了淘宝上几个串口蓝牙模块,功耗在几十到几百uA之间。而且有人说IOS限制休眠时间不能超过1285ms。可是我查到1285ms好像是广播间隔的最大时间,不知道跟我们的需求场景有没有关系。

Zigbee的优点是:
1)淘宝有卖能休眠并定时自动查寻网络的串口模块,平均耗电<10uA
2)能查到一些Zigbee基站(Zigbee转以太网的设备)
缺点是:
1)各家的Zigbee好像协议不太兼容,所以即便买到现成的Zigbee基站好像也不能直接用
2)Zigbee好像不如蓝牙4.0未来发展好。