3) 第一轮预测试,测试实验室对测试结果反馈,开发者修改样品代码。
4) 测试实验室对修改后的样品进行验证,然后开始正式测试。
5) 测试实验室协助开发者完成ZigBee联盟网上认证申请资料的准备和提交。
6) 测试实验室提交正式测试报告给ZigBee联盟。联盟会完成审核并发证
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请教V大,我要路由器协调器烧2007pro,终端烧mesh1.0,有问题吗?因为想的是终端用msp430+cc2520的方式,协调器 路由器用cc2530.或者外挂mcu怎么移植一体mcu的程序
还有就是只找到了exp5438的mesh例程 没找到f2系列的.而且在5438例程里面,好像SPI驱动cc2520的的程序要自己写?
13,如何使用免费的Wireshark做Zigbee Sniffer抓包工具?
可以連結到 dev.ti.com/.../ 的Packet sniffer章節下的wireshark就有詳細說明