This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2538问题!

Other Parts Discussed in Thread: CC2538, CC2530, CC2531

各位好!最近准备用CC2538来做网关,有以下几个硬件问题想咨询一下:

1、CC2538是有提供USB接口的,如果我不用USB口,PIN1-4脚需要做什么处理吗?还是说直接不管就行了?

2、CC2538 JTAG仿真和烧片用到了哪几个管脚?我看TI提供的DEMO上都没有明确提到这个,有没有个参照的datasheet?

3、CC2538的DEMO上天线提供两种,一种倒F天线,另一种SMA接口天线。请问:这两种天线的传输距离怎样?另外我设计成I-PEX接口天线,是否其它参考电路不       变直接用I-PEX替代SMA就行?

4、用CC2538做router,最多能支持多少个CC2530终端设备?

5、外部的32M晶振和32.768KHZ的晶振是否都必须要?

谢谢!

  • 1, PIN 1 USB GND和PIN4 VCC 需要接,PIN2和PIN3可以不接。

    2,CC2538 JTAG是标准的ARM Cotex-M3接口,也支持C-JTAG,具体可以参考 SmartRF06EB User Guide 在TI网上可以下载。

    3,SMA要好于PCB天线。 阻抗匹配需要注意下

    4, 是指整个网络支持,还是单个设备下面可以连接多少CC2530?

    5,32M是必须的,32K可以省,但是如果需要休眠的话,最好把32K也加上去,内部的RC 32KHz会有误差的

  • 你好!

    1、PIN1接GND应该是需要的,我觉得PIN4应该是不需要接的吧,PIN4是USB单独供电的,接在电源的VCC会不会有问题?CC2538会不会出不带USB口的IC,比如说CC2530和CC2531?

    2、DEMO板上用的是SMA接口的外置天线,我改用I-PEX接口的外置天线没问题吧?

    3、一个CC2538下面能最多支持多少个CC2530的终端设备?

    谢谢!