有没有什么标志位,或者什么 协议栈自带的 返回值,能知道接收方是否已经收到数据了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
主要是靠osal_msg_receive函数来接收的 return *uint8 - message information or NULL if no message
/*********************************************************************
* @fn osal_msg_receive
*
* @brief
*
* This function is called by a task to retrieve a received command
* message. The calling task must deallocate the message buffer after
* processing the message using the osal_msg_deallocate() call.
*
* @param uint8 task_id - receiving tasks ID
*
* @return *uint8 - message information or NULL if no message
*/
第一次发帖 问题描述的可能不太清楚
我是想问:点播通信,怎么做到发送数据不会丢失,要做到这样肯定得知道接收方是否接收到数据,没接收到就重发,这样就能做到不丢数据了。
问题是::我怎么知道接收方有没有接收到数据,协议栈有没有这个功能,没有的话只有自己做应答重发机制了。
等待您的回复!