This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PM2功耗与发射功率设置

各位TI员工:

你们好,最近因为要做一个项目,终端EndDevice向协调器发送信息搜集到的温度信息,有如下问题想请各位能不吝指点:

1:EndDevice发送周期为10s,在发射间隙内实现低功耗休眠PM2,这些功能已经实现。现在我想人为修改终端的发射功率,请问发射功率在哪里可以修改?

2:系统正常工作时如果关闭Coordinator,则EndDevice功耗会立即上升到很大,维持约1.2s后又降低约为0,在0mW维持0.3s后又上升,再维持约2s然后又下
降,如此反复下去,实际工作中如果遇到这种情况那终端电池寿命肯定会非常短。之前在做低功耗时我已经在将四个pollrate都置为0了,所以:

(1)请问这个上升的功率是什么原因造成的?

(2)如果我想设置终端检测到连续三次发射不成功就启动一次加入网络的poll,该如何实现呢?

谢谢希望能给以一些建议